enabling uuu support for imx7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

enabling uuu support for imx7

2,680 Views
vishnupratap_si
Contributor I

Hi,

I was trying to create linux kernel firmware binary with uuu support added.

As per the uuu user guide i enabled the FUNCTIONFS in kernel, but when i tried to run this kernel with uuu tool, i get below error -

mkdir: can't create directory 'functions/ffs.utp': Device or resource busy

i checked the functionfs is enabled and in windows it is detected as Functionfs also.

Any help will be appreciated. 

Tags (1)
0 Kudos
Reply
2 Replies

2,248 Views
will_intelli
Contributor III

Hi,

I had this issue, you could try disabling "USB Gadget precomposed configurations" in the kernel configuration.

Will.

0 Kudos
Reply

2,248 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vishnu

latest NXP Linux L4.14.78 uses uuu for programming, so one can check its documentation:

Linux L4.14.78_1.0.0 Documentation
https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_LINUX_DOCS&appType=license&location=null
uuu documentation
https://github.com/NXPmicro/mfgtools/wiki

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply