enable rtsp error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,266件の閲覧回数
vantron
Contributor I

I want enble gstream with rtsp in imx8mqevk, I do step by step as i.MX Linux® User's Guide.

but failed. every time use the command :

root@imx8mqevk:~# gst-launch-1.0 rtspsrc location=rtsp://10.192.241.11:5901 name
=source ! queue ! rtph264depay ! avdec_h264 ! overlaysink source.! queue ! rtpmp
4gdepay ! aacparse ! beepdec ! pulsesink[ 326.824472] random: crng init done
[ 326.827935] random: 7 urandom warning(s) missed due to ratelimiting

WARNING: erroneous pipeline: no element "rtspsrc"
root@imx8mqevk:~# gst-inspect-1.0 rtspsrc
No such element or plugin 'rtspsrc'

how can I go ahead?

0 件の賞賛
返信
1 解決策
3,259件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi vantron,

Did you try to make imx-image-multimedia or imx-image-full?

https://www.nxp.com.cn/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf 

Best Regards

Zhiming

 

元の投稿で解決策を見る

3 返答(返信)
3,260件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi vantron,

Did you try to make imx-image-multimedia or imx-image-full?

https://www.nxp.com.cn/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf 

Best Regards

Zhiming

 

3,240件の閲覧回数
vantron
Contributor I
スポイラ
no, I am not bitbake gstream alone. And it has rtspsrc plugin now.

But there is a new question: I want to use the the vedio compositor on IMX8MQ,but the release note said it not soppurt g2d. And I want to know if there is another way to use  video compositor under 3D?
0 件の賞賛
返信
3,235件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi vantron,

 

IMX8MQ has 2D and 3D compositor. You can know more Chapter5 in i.MX_Reference_Manual.pdf

 

Best Regards

Zhiming

0 件の賞賛
返信