emwin_gui_demo can't be run correctly in flex_spi_nor or xip mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

emwin_gui_demo can't be run correctly in flex_spi_nor or xip mode

1,231 次查看
li-chinwang
Contributor II

I add flex_spi_nor and xip for emwin_gui_demo like in hello_world. After I copy the bin file or use load file, LCD display doesn't  show the image I see in sdram_debug. What's wrong with it?

 

标签 (1)
0 项奖励
回复
3 回复数

1,020 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  You may look at the following:

https://community.nxp.com/message/995816 

Also, perhaps it makes sense to try new SDK, that should be issued soon.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,020 次查看
li-chinwang
Contributor II

I have downloaded newest version of SDK.

In emwin_gui_demo example, there is sdram_debug mode example code.

But it can't used for MP. only flexspi_nor or xip mode can  be MP.

But both these of mode can't work on emwin_gui_demo.

I have done bubble example with flexspi_nor and xip mode. Both two mode have same behavior as it perform in sdram_debug.

Could you deliver the workable emwin_gui_demo example code with flexspi_nor or xip mode

0 项奖励
回复

1,020 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  I meant the release, that is not published yet.

Regards,

Yuri.

0 项奖励
回复