emmc4.5 boot error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

emmc4.5 boot error

2,480 Views
xrz_lam
Contributor I

Dear all,

     I have a strange problem need your help, it was about the EMMC4.5 support

in imx508 android system.    

     It will show below errors every times when the devices bootup from emmc4.5:

     [   10.863246] init: untracked pid 1882 exited

     [   10.883744] init: untracked pid 1886 exited

     [   10.887970] init: untracked pid 1979 exited

    

    Do you know why?How can solve this issue?

   

Here is the reproduce step:

   1.Use the "MfgTool.exe" to update the firmware;

   2.Reset the devices,then bootup the device,it was the first time bootup,in this bootup,it can't appear this problem;

   3.Poweroff the devices,then bootup again,it was the second times bootup,it will appear this problem;

   4.From now,it will appear this problem in every times bootup.

  

Here is the kernel version and android version: 

1.Kernel version:

bash-3.2# cat /proc/version

Linux version 2.6.35.3 (xrz@xrztech171) (gcc version 4.4.3 (GCC) ) #9 PREEMPT Fri Apr 25 10:44:02 HKT 2014

 

bash-3.2# cat cpuinfo

Processor : ARMv7 Processor rev 5 (v7l)

BogoMIPS : 799.53

Features : swp half thumb fastmult vfp edsp neon vfpv3

CPU implementer : 0x41

CPU architecture: 7

CPU variant : 0x2

CPU part : 0xc08

CPU revision : 5

 

 

Hardware : Freescale MX50 Reference Design Platform

Revision : 50011

Serial : 0000000000000000

 

 

 

 

2.Android version: myandroidr10.3.1

 

BTW,

     The attachment files is the log,from "MfgTool.exe" to appear this problem.

Original Attachment has been moved to: emmc4.5_bootup_log.log.zip

Labels (2)
Tags (1)
0 Kudos
Reply
2 Replies

2,257 Views
igorpadykov
NXP Employee
NXP Employee

Hi Qingyuan

i.MX50 ESDHC hardware does not support eMMC4.5,

supports up to 4.4.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,257 Views
xrz_lam
Contributor I

Dear all,here is the log of logcat,Can you help me to check and give me the method to solve this issue? Thanks.

0 Kudos
Reply