elftosb: change startAddress for custom bootloader application

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

elftosb: change startAddress for custom bootloader application

1,701 次查看
e_v_spronsen
Contributor III

I got problems generating bin image files for my application with a custom bootloader.

 I changed the base address of my application  to 0x70080000.

Capture.PNG

From the map file:

.after_vectors.reset
 *(SORT_BY_ALIGNMENT(.isr_vector))
.isr_vector 0x70080000 0x2b8

0x70080308 ResetISR

 

I updated the .bd file:

options {
flags = 0x00;
startAddress = 0x70080000;
ivtOffset = 0x1000;
initialLoadSize = 0x2000;
}

sources {
elfFile = extern(0);
}

section (0)
{
}

When I run elftosb there is no output bin file.

If I run change startAddress  = 0x7000000 back. I got a huge bin file that start at 0x7000000 and jumps to 0x70080000.

So how do I generate a bin file that starts at: 0x70080000?

Thanks!

 

0 项奖励
回复
3 回复数

1,678 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @e_v_spronsen,

Only to confirm, could you let me know the device that you're using and if the custom bootloader used is based in any of the SDK examples/app notes and which one?

Best Regards,

Alexis Andalon

0 项奖励
回复

1,669 次查看
e_v_spronsen
Contributor III

The flash based bootloader I made myself. The lack of documentation is worrisome. I tool a lot of effort to find the info needed.

 

The problem is: I can't make a signed image with start location 0x70080000 with elftosb.exe. The image always starts at 0x70000000.

 

Is the source code available for elftosb?

 

 

 

 

0 项奖励
回复

1,685 次查看
e_v_spronsen
Contributor III

Any suggestions?

0 项奖励
回复