eiQ - Distributed CNN inference

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

eiQ - Distributed CNN inference

2,068 次查看
nullbyte91
Contributor I

Hi Team,

Is it possible to distribute the CNN inference engine to both CPU and GPU using ARMNN/TFLite?
We have our custom network that can run both CPU and GPU. We are looking for an option to distribute the inference engine to both CPU and GPU to get higher FPS.

Regards,
Jegathesan S

0 项奖励
回复
3 回复数

2,043 次查看
Yuri
NXP Employee
NXP Employee

@nullbyte91 
Hello,

   from app team:

  In short, there is no such option in eIQ that can support a CNN to run on both CPU and GPU at the same time. 

  However, it's possible from the application level to achieve that. As you can find in the eIQ demo, we can switch CPU/GPU inference in this application:

https://source.codeaurora.org/external/imxsupport/pyeiq/tree/eiq/apps/switch_video/switch_video.py?h...

   Let's assume that GPU inference will take 0.1s to finish one frame and CPU inference will take 0.5s to finish one frame. We can give frame 6, 12 to CPU inference thread to calculate and frame 1-5, 7-11 to GPU inference thread to calculate. By the end of 1 second, we will have totally 12 frames finished inference. Comparing to use GPU only, it can raise FPS from 10 to 12.

    But in reality, it's not easy to keep perfect sync between CPU and GPU. And usually GPU is much faster ,comparing to CPU, to run CNN inference. Therefore it may not be worthy to include CPU but adding this SW complexity.

 

Regards,
Yuri,

0 项奖励
回复

2,052 次查看
nullbyte91
Contributor I

Hi @Yuri, 

I'm using MX 8QuadMax.

0 项奖励
回复

2,059 次查看
Yuri
NXP Employee
NXP Employee

@nullbyte91 
Hello,

   What i.MX device is used in the case?

Regards,
Yuri.

0 项奖励
回复