eboot_ivt.sb doesn't support Nand flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eboot_ivt.sb doesn't support Nand flash

1,631件の閲覧回数
RichardXiao
Contributor I

MFGtool update Wince into Nand flash failed;

 

boot from SD card, eboot can't find Nand flash;

 

I download wince image from freescale website;

 

so, result is that eboot doesn't support nand flash ??

ラベル(1)
0 件の賞賛
返信
1 返信

1,319件の閲覧回数
RichardXiao
Contributor I

Table 7. BSP Known Issues/Limitations


Limitation/Issue :If NAND Flash was programmed by other OS or program,
WinCE BSP may have problem read/write NAND as normal.

Workaround:Perform a low-level NAND format in EBOOT.

0 件の賞賛
返信