eMMC5.0 Boot with Bus Width=8bit access for i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

eMMC5.0 Boot with Bus Width=8bit access for i.MX6

跳至解决方案
3,502 次查看
yuuki
Senior Contributor II

Dear all,

Our customer uses eMMC5.0 device.
And they make a system boot from eMMC with Bus Width=8bit(BOOT_CFG2[7:5]=010).

In this case, system can not boot.

When Bus Width is set to 4bit(BOOT_CFG2[7:5]=001) and U-Boot is set as 4bit, system is able to boot.
However, boot speed is very slow.

Is there a way to be accessed by 8 bits at booting from eMMC5.0 device?

May I have advice?

Best Regards,
Yuuki

标签 (1)
0 项奖励
回复
1 解答
2,747 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,748 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
2,750 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

what processor and SD port used in the case ?

Best regards

igor

0 项奖励
回复
2,750 次查看
yuuki
Senior Contributor II

Dear Igor-san,

Thank you for your support.

Prosessor is i.MX6 solo(MCIMX6S5EVM10AB).

SD port is SD4.

Please advise of your findings.

Best Regards,

Yuuki

0 项奖励
回复
2,750 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

8-bit eMMC is working fine on i.MX6 reference

board Sabre SPF-27392  p.5

i.MX6_SABRE_SDP_DESIGNFILES

probably there are layout errors or issues

related to layout (signtal integrity), one can try

to check signals by oscilloscope.

Best regards

igor

0 项奖励
回复
2,750 次查看
rahulsoni
Contributor II

Hello Igor,

I have the same configuration as Yuuki. i.MX6 Solo and eMMC 5.0 @ SD4 port. I see the eMMC on kernel but can not see eMMC on u boot due to which I'm not able to boot my device over eMMC. Below are my boot configuration settings-

CFG1[7:0]- 01101000

CFG2[7:0]- 11011000

Please help me to resolve this problem.

Thanks in advance.

0 项奖励
回复