eMMC write/read test failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

eMMC write/read test failed

1,088 次查看
jasonedn
Contributor II

When the example mmccard_freertos runs on the RT1020EVK, the first write/read test passed but the following tests failed . Below are logs:

Read/write the card continuously until encounter error......

Write/read block test: start block#=2, block count=1
Write 1 data blocks......
Read 1 data blocks......
Compare the read/write content......
The read/write content is consistent.

Write/read block test: start block#=2, block count=5
Write 5 data blocks......
Read 5 data blocks......
Compare the read/write content......
The read/write content is consistent.

Erase data groups......
Erase blocks ok

Input 'q' to quit read/write/erase process.
Input other char to read/write/erase data blocks again.
1
Write/read block test: start block#=2, block count=1
Write 1 data blocks......  <It was stuck here>

 

 If the tests continue to run, they succeed. It seems the eMMC device goes to sleep if there is no any operations on eMMC, and it won't respond anymore. Is this tur? If yes, how to wakeup the device again? Thanks.

0 项奖励
回复
1 回复

1,083 次查看
nxf63675
NXP TechSupport
NXP TechSupport

Hi jasonedn,

 

Please post this on the i.MX RT community, this is for i.MX processors.

 

Regards,

Israel H.

0 项奖励
回复