eMMC list

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMMC list

Jump to solution
2,948 Views
jiejia
Contributor III

board: mx6q_sabresd    BSP:L3.0.35

The eMMC (SDIN5C2-8G) is no longer possible in market. Is there a replace emmc which it's pin-to-pin compatible?

Best regards,

Labels (2)
0 Kudos
Reply
1 Solution
2,348 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi jie,

The i.MX6 processor supports the MMC System Specification version 4.2/4.3/4.4/4.41. Any device, compatible with these specifications, can be used with i.MX6. Here I share the emmc with you:

http://pan.baidu.com/s/1bTOLGE

Password:cf49
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,348 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi jie,

I will confirm it for you. Please have a wait.

Have a nice day

Dan

0 Kudos
Reply
2,348 Views
jiejia
Contributor III

Hi Dan,

   Can you find such a emmc?

0 Kudos
Reply
2,349 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi jie,

The i.MX6 processor supports the MMC System Specification version 4.2/4.3/4.4/4.41. Any device, compatible with these specifications, can be used with i.MX6. Here I share the emmc with you:

http://pan.baidu.com/s/1bTOLGE

Password:cf49
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply