eMMC list

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,924件の閲覧回数
jiejia
Contributor III

board: mx6q_sabresd    BSP:L3.0.35

The eMMC (SDIN5C2-8G) is no longer possible in market. Is there a replace emmc which it's pin-to-pin compatible?

Best regards,

ラベル(2)
0 件の賞賛
返信
1 解決策
2,324件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi jie,

The i.MX6 processor supports the MMC System Specification version 4.2/4.3/4.4/4.41. Any device, compatible with these specifications, can be used with i.MX6. Here I share the emmc with you:

http://pan.baidu.com/s/1bTOLGE

Password:cf49
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,324件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi jie,

I will confirm it for you. Please have a wait.

Have a nice day

Dan

0 件の賞賛
返信
2,324件の閲覧回数
jiejia
Contributor III

Hi Dan,

   Can you find such a emmc?

0 件の賞賛
返信
2,325件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi jie,

The i.MX6 processor supports the MMC System Specification version 4.2/4.3/4.4/4.41. Any device, compatible with these specifications, can be used with i.MX6. Here I share the emmc with you:

http://pan.baidu.com/s/1bTOLGE

Password:cf49
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信