eMMC CLK Voltage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eMMC CLK Voltage

4,516件の閲覧回数
coilnpark
Contributor IV

Hi all,

I am developping custom board by using SABRESD board.

I have a simpmle question.

As I know, emmc CLK voltage is proper 3.3V or 1.8V according to the VCC or VCCQ voltage.

However, my board CLK voltage is 5V as below the picture.

When I checked SD card CLK, it was also 5V.

I am using usdhc2, 4 (eMMC is using usdhc4)

Anybody can help me?

eMMC CLK-UP.png

 

 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

4,488件の閲覧回数
coilnpark
Contributor IV

Hi, igor

I refered the scehmetic of SABRESD NXP_SPF-27392_C3. It used just GEN3V3.

Do I have to use  "NVCC_NANDF" Power?

 

[SPF-27392_C3]

coilnpark_0-1625638600454.png

[My board]

coilnpark_1-1625638629838.png

 

 

0 件の賞賛
返信

4,507件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Coiln

 

from i.MX6Q side voltage should be as described in Table 96. 21 x 21 mm Functional Contact Assignments, column "Power Group"

i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet

If it is 5V, probably it is shorted to some other signal.

 

Best regards
igor

0 件の賞賛
返信

4,502件の閲覧回数
coilnpark
Contributor IV

Hi igor

Thank you for your prompt reply.

I also tested sdcard clk of SABRESD kit.

The sdcard clk voltage was 4.3V

Even I will check our board for high voltage, SABRESD kit voltage is also weird.

Could you check it?

Best regards,

Colin Park

20210706_173336.jpg

0 件の賞賛
返信