eIQ based sample application-Tflite face recognition CPP app stuck with compilation errors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eIQ based sample application-Tflite face recognition CPP app stuck with compilation errors

1,118件の閲覧回数
rmani0029
Contributor I

I am facing the following compilation errors while trying to compile the eiq tflite based face_recognition sample application through the latest built fsl-imx-wayland-glibc-x86_64-imx-image-full-aarch64-toolchain-5.4-zeus SDK.

Error logs :

---------------------------

imx8@imx8:~/eIQ_NXP/eiq_sample_apps/examples-tflite/face_recognition/src$ make -f Makefile.linux
aarch64-poky-linux-g++ --sysroot=/opt/fsl-imx-wayland/5.4-zeus-new/sysroots/aarch64-poky-linux -o FaceRecognition -I /opt/fsl-imx-wayland/5.4-zeus-new/sysroots/aarch64-poky-linux/usr/include/tensorflow/lite/tools/make/downloads/flatbuffers/include/ face_recognition.cpp face_detect_helpers.cpp -ltensorflow-lite -lpthread -lrt -ldl -g -lopencv_objdetect -lopencv_highgui -lopencv_imgproc -lopencv_core -lopencv_videoio -lopencv_imgcodecs
/opt/fsl-imx-wayland/5.4-zeus-new/sysroots/x86_64-pokysdk-linux/usr/libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/9.2.0/real-ld: cannot find -ltensorflow-lite
collect2: error: ld returned 1 exit status
Makefile.linux:13: recipe for target 'FaceRecognition' failed
make: *** [FaceRecognition] Error 1

So, Kindly help me on how to solve those compilation errors.

Regards,

Manikandan.R

0 件の賞賛
返信
1 返信

1,102件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello mani0029,

Generally this problem occurred when we have called a function which has not been define in the program file, so to sort out this problem check whether have you called such function which has not been define in the program file. or you miss to install some package.

 

Regards

 

0 件の賞賛
返信