eCSPI connection with 4bit data mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eCSPI connection with 4bit data mode

1,582件の閲覧回数
ko-hey
Senior Contributor II

Hi

I am designing a system with i.MX6 processor and planning to boot from sirial flash(256 or 512Mbit).

But I could not find any description about 4 bit mode.

So I have a question about eCSPI.

Can I use in 4 bit data mode in one of the channels?

If yes, please let me know about a recommended connection between serial flash and i.MX6.

Please clarify,

Sincerely

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,503件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

current i.MX6x do not support quadSPI, it will be supported in new i.MX6SoloX processor.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,503件の閲覧回数
ko-hey
Senior Contributor II

Hi Igor

Thank you for your quick reply.

I understood.

Best Regards,

ko-hey

0 件の賞賛
返信