Hi m.c.
yes, it supports: from sect.40.4.1 Input Parallel Display Ports IMX6SDLRM :
One or Two (DI0, DI1) parallel RGB input ports are supported (configurable)...
sect.40.4.2 Output LVDS Ports:
There are 2 LVDS channels. These outputs are used to communicate RGB data and
controls to external LCD displays.
• Separate 2 channel output (2 input sources from IPU).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------