drive strength

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

drive strength

2,972 Views
geethar
Contributor II

How to change the drive strength of mobile DDR?

Labels (1)
0 Kudos
Reply
5 Replies

2,704 Views
geethar
Contributor II

How can i access the mobile DDR mode register and extended mode register address?

How to set mode register in DDR?

0 Kudos
Reply

2,704 Views
geethar
Contributor II

part number for my micron mobile ddr is MT46H32M16LFBF-6 IT:C

0 Kudos
Reply

2,704 Views
Yuri
NXP Employee
NXP Employee

  According to the MT46H32M16LFBF  Datasheet, Extended Mode Register (EMR)

controls in particular drive strength. The EMR is programmed via the LOAD MODE REGISTER
command with BA0 = 0 and BA1 = 1. EMR bits 5,6,7 define memory drive strength.

< http://www.micron.com/~/media/Documents/Products/Data%20Sheet/DRAM/Mobile%20DRAM/Low-Power%20DRAM/LP... >



IMX23 provides EMR writing via setting bit field HW_DRAM_CTL38 [EMRS1_DATA] and

setting HW_DRAM_CTL09 [ WRITE_MODEREG ].

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,704 Views
Yuri
NXP Employee
NXP Employee

What is modile DDR (part number, Datasheet) ?

0 Kudos
Reply

2,704 Views
Yuri
NXP Employee
NXP Employee

   Please use DDR Mode registers (Extended Mode Register) to configure DDR

Output Drive Strength during DDR initialization.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply