download uboot success but serial console output nothing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

download uboot success but serial console output nothing

跳至解决方案
1,101 次查看
13126507966
Contributor II

hello

we custom a board according to imx8mq_evk board, but the DDR isn't the same. I modify the DDR configure with mscale_ddr_tool_v310,and download uboot successful,you can see the uboot_down_process.log.After this we config BOOT_MODE=0b10(internal boot),

BOOT_CFG[0]=0,

BOOT_CFG[1]=0,

BOOT_CFG[3:2]=00,

BOOT_CFG[6:4]=010,

BOOT_CFG[7]=1,

BOOT_CFG[8]=1,

BOOT_CFG[9]=0,

BOOT_CFG[11:10]=00,

BOOT_CFG[15:12]=0010

and then power on the serial console has nothing output.Can you give me a hand? thanks very much!

0 项奖励
回复
1 解答
1,036 次查看
13126507966
Contributor II

I solve this problem,the BOOT_CFG register config 0x2002, so the board is running.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,037 次查看
13126507966
Contributor II

I solve this problem,the BOOT_CFG register config 0x2002, so the board is running.

0 项奖励
回复