does the i.mx93 support opengl?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

does the i.mx93 support opengl?

ソリューションへジャンプ
3,984件の閲覧回数
cbrake
Contributor III

Does the i.MX93 support OpenGL (Qt)? 

How does the graphics performance compare to something like the i.MX 8M Nano?

Thanks!

タグ(1)
0 件の賞賛
返信
1 解決策
3,908件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @cbrake!

The iMX 93 only has a 2D GPU and is not compatible with OPENGL.

The iMX 95 is compatible with OPENGL.

Best Regards!

Chavira

元の投稿で解決策を見る

3 返答(返信)
3,963件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @cbrake!
Thank you for contacting NXP Support!

The iMX93 supports QT.

To see all the features of our BSP you can consult our Linux Release Notes:


We don’t provide comparisons between processors you have to do your proper tests according to your application.

Best Regards!

Chavira

0 件の賞賛
返信
3,934件の閲覧回数
cbrake
Contributor III

Thanks for the reply. Qt provides graphics rendering through openGL or a software renderer. My question specifically is does the i.MX93 have a GPU that provides OpenGL ES support? 

0 件の賞賛
返信
3,909件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @cbrake!

The iMX 93 only has a 2D GPU and is not compatible with OPENGL.

The iMX 95 is compatible with OPENGL.

Best Regards!

Chavira