do not enter recovery

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

do not enter recovery

2,677件の閲覧回数
donghyunkim
Contributor III

bsp : android_N7.1.1_1.0.0

board : i.MX6qp sabresd

reference document : Android_Frequently_Asked_Questions.pdf (8 How do I enter the Android recovery mode manually?)

"reboot recovery" command does not enter recovery in Android N7.1.1

but, it works in factory reset menu in settings.

and, one strange...

after doing the "reboot ..." command, output "Reset cause: POR" message in u-boot.

is "Reset cause: WDOG" true?

to my recollection, it seems that "Reset cause: WDOG" message in Android gingerbread.

ask for advice.

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,429件の閲覧回数
marcowang
Contributor II

Hi DongHyun Kim,

Could you please tell me how to set BCB ? Tks

0 件の賞賛
返信

2,429件の閲覧回数
JayTu
NXP Employee
NXP Employee

Factory reset is mandatory but not reboot recovery.

It shows WDOG since reboot is done by watchdog.

0 件の賞賛
返信

2,429件の閲覧回数
donghyunkim
Contributor III

Hi, JayTu.

This problem occurred because did not set BCB.

It's solved.

Thanks!!

0 件の賞賛
返信