do_configure: QA Issue: libxsettings-client: Recipe file does not have license file information

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

do_configure: QA Issue: libxsettings-client: Recipe file does not have license file information

3,259件の閲覧回数
analogicstechin
Contributor III

can please solve my issue , facing while compiling .

$ bitbake fsl-image-gui

ERROR: libxsettings-client-0.17-r5.1 do_configure: QA Issue: libxsettings-client: Recipe file does not have license file information (LIC_FILES_CHKSUM) [license-checksum]
ERROR: libxsettings-client-0.17-r5.1 do_configure: Fatal QA errors found, failing task.
ERROR: libxsettings-client-0.17-r5.1 do_configure: Function failed: do_qa_configure
ERROR: Logfile of failure stored in: /media/ashok/NXPIMX6/fsl-community-bsp/imx6ullevk-ptc/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/libxsettings-client/0.17-r5.1/temp/log.do_configure.14490
ERROR: Task 6397 (/media/ashok/NXPIMX6/fsl-community-bsp/sources/meta-openembedded/meta-gpe/recipes-graphics/libxsettings-client/libxsettings-client_0.17.bb, do_configure) failed with exit code '1'

ラベル(1)
0 件の賞賛
返信
1 返信

2,495件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信