distro backend for headless device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

distro backend for headless device

1,923 Views
davidvescovi
Contributor V

I am planning on building a headless embedded device.

I need gstreamer as I will be doing camera capture but I do have a display.

Normally I would use xwayland or frambuffer as a backend but because this is headless I am wondering if one of the other distro's without a windowing backend might be a better choice? What would be a better selection? Do these more "minimal" distros still support gstreamer?

0 Kudos
Reply
2 Replies

1,865 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello David,

Gstreamer is part of Multimedia plugins package, you need any multimedia backend to star to work with it, or you can have it in core-image-minimal but you will have to add all the resources they need.

Regards

0 Kudos
Reply

1,478 Views
moose
Contributor IV

This post doesn't really answer my distro question. Do we really need wayland, weston, etc. to run a headless hardware? Could you please specify the recommended distro configuration?

0 Kudos
Reply