/dev/ttyLP1 is not created for Bluetooth

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

/dev/ttyLP1 is not created for Bluetooth

跳至解决方案
4,449 次查看
vinothkumars
Senior Contributor IV

Hi All,

 

I unable to create the serial port (/dev/ttyLP1) for bluetooth.

 

Please find my configuration,

&lpuart1 { /* BT */
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lpuart1>;
resets = <&modem_reset>;
status = "okay";

/* Enable bt driver for marvel uart8987 */
bluetooth {
compatible = "mrvl,88w8897";
status = "okay";
};
};

 

I unable to find the tty ,

/sys/devices/platform/bus@5a000000/5a070000.serial

 

 

 

 

 

 

Regards,
Vinothkumar Sekar
1 解答
4,256 次查看
vinothkumars
Senior Contributor IV

Hi

 

The issue is resolved long time back. To connect with devices we should add the services like audio and file transfer (ex: pactl, obexftp)

 

 

Regards,
Vinothkumar Sekar

在原帖中查看解决方案

0 项奖励
回复
7 回复数
4,143 次查看
josephzhou1
Contributor V

yes

Best Regards,
Joseph Zhou Jianhui / Senior Embedded Software Engineer, Singapore
0 项奖励
回复
4,430 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

what bsp used in the case.

 

Best regards
igor

4,404 次查看
vinothkumars
Senior Contributor IV

Hi @igorpadykov 

 

Please find my response,

[bluetooth]# connect D2:33:E4:49:05:51
Attempting to connect to D2:33:E4:49:05:51

I able to pair with my mobile but not able to connect

I am using Bluetooth 5.0 (Classic as well as LE).

 

Regards,
Vinothkumar Sekar
4,399 次查看
igorpadykov
NXP Employee
NXP Employee
4,423 次查看
vinothkumars
Senior Contributor IV

Thank you @igorpadykov ,

 

I am working IMX8QM Custom platform with Yocto BSP (L5.10) version with Marvell chip for Bluetooth which is using UART interface.

Regards,
Vinothkumar Sekar
4,257 次查看
vinothkumars
Senior Contributor IV

Hi

 

The issue is resolved long time back. To connect with devices we should add the services like audio and file transfer (ex: pactl, obexftp)

 

 

Regards,
Vinothkumar Sekar
0 项奖励
回复
4,154 次查看
Jose1985
Contributor IV

Hi @vinothkumars ,

I hope you were able to add 8997 module with iMX8QM MEK board. Can you help me how you made Bluetooth working using 8997 pcie module?

 

Best regards,

Jose1985