/dev/fb0 relation to IPU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

/dev/fb0 relation to IPU

3,470件の閲覧回数
robertspriggs
Contributor I

Hi,

I'm using a custom i.MX6dl board with Linux. I have found using GStreamer sometimes that if I pause playback, then capture /dev/fb0, the image I get is a frame before what I see paused on the screen coming out of the IPU. Can anyone give me an idea what might be happening?

-Rob.

ラベル(5)
0 件の賞賛
返信
3 返答(返信)

3,339件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rob

what bsp/gstreamer used in the case, please try with nxp bsps described on

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/?id=rel_imx_4.1.15_2.0.0_ga&h=imx_4.1.1... 

and gstreamer usage in sect. 7 Multimedia attached Linux Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,339件の閲覧回数
robertspriggs
Contributor I

A new BSP is not an option. I built the i.MX GStreamer plugins from source code I found here: GitHub - Freescale/gstreamer-imx: GStreamer 1.0 plugins for i.MX platforms 

After further investigation, I've found that pausing video often causes a jump of several frames ahead (sometimes 5 or 6) for what is on screen, but /dev/fb0 seems to contain the correct frame where the video SHOULD be paused. I think unless someone has an answer, my best recourse is to analyze the i.MX plugin source code. For our application we need a pause to be a true playback freeze.

0 件の賞賛
返信

3,339件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

gstreamer-imx plugins are not nxp software, it is supported through community,

please check maintainer of gstreamer-imx plugins mentioned on
https://community.nxp.com/thread/445732

difference between community gstreamer-imx plugins and nxp gstreamer plugins

described on

trac.gateworks.com/wiki/Yocto/gstreamer

Best regards
igor

0 件の賞賛
返信