ddr calibration failure in imx6dl

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ddr calibration failure in imx6dl

2,393 Views
abdulhussain
Contributor III

Hi,

I am trying to run ddr callibration in imx6dl and it is getting failed with the following error,

# DDR_Stress_Tester.exe -t mx6x -df imx6dl-custom.inc
MX6DL opened.
HAB_TYPE: DEVELOP
rom_write: reading HAB ack failed 0x00000000
ROM Write failed, addr: 0x021b001c
Write dcd failed.

#

We are using DDR3-1333 part no: IS46TR16256A-15HBLA2-TR.

Please find the attached ddr3 script aid configuration.

Kindly help us to find out what is wrong with the configuration.

Regards,

Abdul

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,068 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abdul

please try latest gui version of tool, use description in presentation and look at FAQ on below link

Q. I see an error message that states "ERROR: DCD addr is out of valid range.",

i.MX6/7 DDR Stress Test Tool V2.80 

https://community.nxp.com/docs/DOC-331528 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,068 Views
abdulhussain
Contributor III

Hi Igor,

Even i tried the latest version of ddr stress tool, still i am getting the same error.

Can you point out me where to download the latest ddr3 programming aid excel file for imx6dl processor?

Regards,

Abdul

0 Kudos
Reply

2,068 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abdul

please look at

i.MX6ULL_LPDDR2_Script_Aid 

you can try to comment line which caused error as in

https://community.nxp.com/message/937539 

Best regards
igor

0 Kudos
Reply