custom user interface Android / Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

custom user interface Android / Linux

1,857 Views
alderlopez
Contributor I

I'm working with some tools imx53, imx6 I would like to know where I should start to develop an interface based on Android or Linux for such as a touch system to control some processes, I mean the custom UI to not show the traditional desktop Android or Linux

0 Kudos
Reply
2 Replies

1,694 Views
Yuri
NXP Employee
NXP Employee

  You may look at section UI Build Tools (6) on the Summary page :

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&fpsp=1&tab=Design_Tools_Tab


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,694 Views
alderlopez
Contributor I

Hi Yuri,

thanks a lot,  I am reading, and I see one of the environments is using QT, among others.

I'm looking for some free options too, if they exist.

0 Kudos
Reply