creating an image with dm-verity-initramfs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

creating an image with dm-verity-initramfs

4,791 次查看
greeran
Contributor IV

I am trying to create a full chain of trust boot. the secure boot was successful but i am having problems with dm-verity on the rootfs. i added configuration to the conf/locol.conf

IMAGE_INSTALL_append = " lvm2 cryptsetup "

IMAGE_FEATURES_append = " read-only-rootfs "

DM_VERITY_IMAGE = "fsl-image-qt5"
DM_VERITY_IMAGE_TYPE = "ext4"

IMAGE_CLASSES += " dm-verity-img "

IMAGE_BOOT_FILES_append = " fitImage-${INITRAMFS_IMAGE}-${MACHINE}-${MACHINE}"

INITRAMFS_IMAGE = "dm-verity-image-initramfs"
INITRAMFS_FSTYPES = "cpio.gz"
INITRAMFS_IMAGE_BUNDLE = "1"

in the deploy images i see the

dm-verity-initramfs cpio, Image.initramfs bin,  rootfs.ext4.verity file

but when i deploy the fsl-image-qt5-imx8mm-var-dart.tar.gz file to the SD card i do not see that the initramfs or the dm-verity is working.

i thought the BUNDLE option binds the initfamfs to the oginal Image and the verity rootfs is bundled to the tar.gz that is deployed to the the SDCard

 

标签 (1)
0 项奖励
回复
1 回复

4,779 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @greeran 

As this feature is supported by Yocto layer, you can post this issue in yocto community.

Reference link: https://lists.yoctoproject.org/g/yocto/message/49112

0 项奖励
回复