core-image-full-cmdline build failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

core-image-full-cmdline build failed

2,422 Views
brucesun
Contributor III

Hi,

I can build core-image-minimal image without any problem. But when I tried to build core-image-full-cmdline, I got an error and stopped. has anyone experienced this kind of issue?

bruce@bruce-XPS-8700:~/mc3000-working/fsl-release-bsp/build-q$ bitbake core-image-full-cmdline

Loading cache: 100% |#########################################################################################################################################| ETA:  00:00:00

Loaded 2524 entries from dependency cache.

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION        = "1.24.0"

BUILD_SYS         = "x86_64-linux"

NATIVELSBSTRING   = "Ubuntu-14.04"

TARGET_SYS        = "arm-poky-linux-gnueabi"

MACHINE           = "imx6qsabreauto"

DISTRO            = "poky"

DISTRO_VERSION    = "1.7"

TUNE_FEATURES     = "arm armv7a vfp neon callconvention-hard cortexa9"

TARGET_FPU        = "vfp-neon"

meta             

meta-yocto        = "(nobranch):f20e4c0cf6ddb29a1aad6e7b095e1472e81d330c"

meta-oe          

meta-multimedia   = "(nobranch):7bbacd0023fa1111da94ba0b2aafd7d872301ffe"

meta-fsl-arm      = "(nobranch):b74e5e690d8d4e149ea9de3f0fcca37bad93935f"

meta-fsl-arm-extra = "(nobranch):b32528c10caac5e85f2b5efe0e5b95322dd68ace"

meta-fsl-demos    = "(nobranch):48cb0bcdd226d2e7eee1fdc222713e1dff93342c"

meta-fsl-arm     

meta-fsl-demos    = "(nobranch):9a2973abf0d1de9742561c3af57de7b8cba7063a"

meta-browser      = "(nobranch):63963cc56c8d0291779693e62b66cb16e5c86883"

meta-gnome       

meta-networking  

meta-python      

meta-ruby        

meta-filesystems  = "(nobranch):7bbacd0023fa1111da94ba0b2aafd7d872301ffe"

meta-qt5          = "(nobranch):41c5daa84af4466bfc9aa61f6f772c68470a628b"

meta-fsl-qt5     

meta-fsl-bluez    = "(nobranch):9a2973abf0d1de9742561c3af57de7b8cba7063a"

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

ERROR: Function failed: nettools_do_patch (log file is located at /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/temp/log.do_patch.22294)

ERROR: Logfile of failure stored in: /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/temp/log.do_patch.22294

Log data follows:

| DEBUG: Executing python function do_patch

| DEBUG: Executing shell function nettools_do_patch

| No patch removed

| patching file debian/rules

| patching file debian/install

| patching file debian/config.h

| patching file debian/compat

| patching file debian/config.make

| patching file debian/copyright

| patching file debian/watch

| patching file debian/README.source

| patching file debian/control

| patching file debian/changelog

| patching file debian/patches/CVS-20081003-config.in_sync.patch

| patching file debian/patches/Bug#345331-socket_overflow.patch

| patching file debian/patches/netstat.c-local_changes.patch

| patching file debian/patches/CVS-20070316-netstat.c_sync.patch

| patching file debian/patches/netstat.c-assorted_changes.patch

| patching file debian/patches/CVS-20061011-includes_sync.patch

| patching file debian/patches/Bug#254243-netstat.c-wide-opt.patch

| patching file debian/patches/CVS-20071202-rarp.c_sync.patch

| patching file debian/patches/CVS-20030911-nameif.c_sync.patch

| patching file debian/patches/Bug#569509-iface_overflow.patch

| patching file debian/patches/series

| patching file debian/patches/CVS-20051204-slttach.c_sync.patch

| patching file debian/patches/local-manpages.patch

| patching file debian/patches/lib_local_changes.patch

| patching file debian/patches/CVS-20081003-statistics.c_sync.patch

| patching file debian/patches/CVS-20020730-route.c_opts_64.patch

| patching file debian/patches/CVS-20081002-ifconfig.c_sync.patch

| patching file debian/patches/CVS-20031011-hostname.c_sync.patch

| patching file debian/patches/CVS-20051204-arp.c_sync.patch

| patching file debian/patches/CVS-20081002-manpages_sync.patch

| patching file debian/patches/Add_missing_headers.patch

| patching file debian/patches/CVS-20060927-mii-tool.c_sync.patch

| patching file debian/patches/translations.patch

| patching file debian/patches/proper-uts-check.patch

| patching file debian/patches/CVS-20061011-ipmaddr.c_buffer_overflow.patch

| patching file debian/patches/CVS-lib_sync.patch

| patching file debian/patches/fix-fprintf.patch

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/CVS-20020730-route.c_opts_64.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/CVS-20030911-nameif.c_sync.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/CVS-20031011-hostname.c_sync.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/CVS-20051204-arp.c_sync.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/CVS-20051204-slttach.c_sync.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/CVS-20060927-mii-tool.c_sync.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/CVS-20061011-includes_sync.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/CVS-20061011-ipmaddr.c_buffer_overflow.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/CVS-20070316-netstat.c_sync.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/CVS-20071202-rarp.c_sync.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/CVS-20081002-ifconfig.c_sync.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/CVS-20081003-statistics.c_sync.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/CVS-lib_sync.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/CVS-20081003-config.in_sync.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/CVS-20081002-manpages_sync.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/netstat.c-assorted_changes.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/Bug#254243-netstat.c-wide-opt.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/netstat.c-local_changes.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/translations.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/lib_local_changes.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/local-manpages.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/Bug#345331-socket_overflow.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/Bug#569509-iface_overflow.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/Add_missing_headers.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/proper-uts-check.patch is already applied; check your series file

| Patch /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/net-tools-1.60/debian/patches/fix-fprintf.patch is already applied; check your series file

| WARNING: exit code 1 from a shell command.

| DEBUG: Python function do_patch finished

| ERROR: Function failed: nettools_do_patch (log file is located at /home/bruce/mc3000-working/fsl-release-bsp/build-q/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/net-tools/1.60-25-r0/temp/log.do_patch.22294)

ERROR: Task 1634 (/home/bruce/mc3000-working/fsl-release-bsp/sources/poky/meta/recipes-extended/net-tools/net-tools_1.60-25.bb, do_patch) failed with exit code '1'

NOTE: Tasks Summary: Attempted 1830 tasks of which 1820 didn't need to be rerun and 1 failed.

Waiting for 0 running tasks to finish:

Summary: 1 task failed:

  /home/bruce/mc3000-working/fsl-release-bsp/sources/poky/meta/recipes-extended/net-tools/net-tools_1.60-25.bb, do_patch

Summary: There was 1 ERROR message shown, returning a non-zero exit code.

bruce@bruce-XPS-8700:~/mc3000-working/fsl-release-bsp/build-q$

Regards,

Bruce

Labels (2)
0 Kudos
Reply
3 Replies

1,903 Views
BiyongSUN
NXP Employee
NXP Employee

Untitled.png

0 Kudos
Reply

1,903 Views
brucesun
Contributor III

Hi Biyong,

Do you mean ONLY the images listed in your table are valid for freescale YOCTO release?

Regards,

Bruce

0 Kudos
Reply

1,903 Views
BiyongSUN
NXP Employee
NXP Employee

yes.

The list is we have done the QA.

0 Kudos
Reply