connection fail to git server..

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

connection fail to git server..

2,048件の閲覧回数
seyoungkim
Contributor II

Hi everyone.

in a yocto repo download step making error

->>>  git://git.freescale.com/imx/linux-imx.git.  and u-boot-imx  too..

it makes error message "connection refusd."

i tried change network access-point to my phone. but it makes same error.

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,891件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi seyoung

please look at

[meta-freescale] Issue with freescale git server at git.freescale.com 

[meta-freescale] [PATCH] linux-imx: Change git repository URL 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,891件の閲覧回数
rensdol
Contributor I

Is someone working on this?  I have this error trying to build the manufacturing tools for imx7dsabresd.

ERROR: u-boot-imx-mfgtool-2016.03-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 128, output:
Cloning into bare repository '/home/rens/yocto/fsl-release-bsp/downloads//git2/git.freescale.com.imx.uboot-imx.git'...
fatal: read error: Connection reset by peer.

Sorry wrong error this was a local network error,  

The build is stuck at

Currently 2 running tasks (1471 of 1538):
0: linux-imx-4.1.15-r0 do_fetch (pid 2733)
1: mfgtool-linux-imx-4.1.15-r0 do_fetch (pid 2734)

Is there a dedicated forum thread for git server status and error reports?

Regards

Rens

0 件の賞賛
返信