configure static ip on imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

configure static ip on imx6

Jump to solution
4,595 Views
davidshoham
Contributor II

Hi,

I installed the basic rootfs from the"L3.0.35_12.09.01_GA_images_MX6Q" packages. I am trying to configure a static ip permanently and have n idea how to do this. In the meantime I am configuring the ip with 'ifconfig' every time I switch on the card.

Thanks,

David.

Labels (1)
1 Solution
3,068 Views
fabio_estevam
NXP Employee
NXP Employee

You can pass the IP you want in the kernel command line (from the bootloader) like this:

ip=192.168.1.102:192.168.1.101

,where

192.168.1.101: is the serverip IP address

192.168.1.102: is the target (mx6 board) IP address

Regards,

Fabio Estevam

View solution in original post

2 Replies
3,068 Views
davidshoham
Contributor II

Thanks!

0 Kudos
Reply
3,069 Views
fabio_estevam
NXP Employee
NXP Employee

You can pass the IP you want in the kernel command line (from the bootloader) like this:

ip=192.168.1.102:192.168.1.101

,where

192.168.1.101: is the serverip IP address

192.168.1.102: is the target (mx6 board) IP address

Regards,

Fabio Estevam