Hi NXP,
[Description]
We are using GPIO0_IO00 as WiFi enable pin. We are trying to make this pin HIGH from uboot dts.
Below are the changes we tried:
diff --git a/arch/arm/dts/imx8mp-evk.dts b/arch/arm/dts/imx8mp-evk.dts
index f6f33cb769..d7b3998f40 100644
--- a/arch/arm/dts/imx8mp-evk.dts
+++ b/arch/arm/dts/imx8mp-evk.dts
+ wifi {
+ pinctrl-names = "default";
+ pinctrl-0 = <&pinctrl_wifi_regon>;
};
pcie0_refclk: pcie0-refclk {
@@ -939,4 +944,10 @@
MX8MP_IOMUXC_GPIO1_IO02__WDOG1_WDOG_B 0x166
>;
};
+
+ pinctrl_wifi_regon: wifi_regon {
+ fsl,pins = <
+ MX8MP_IOMUXC_GPIO1_IO00__GPIO1_IO00 0x40
+ >;
+ };
};
[Observations]
The pin remains LOW on probing.
Can you please help us to identify where are doing wrong.?
Also, are we programming the correct offset value (MX8MP_IOMUXC_GPIO1_IO00__GPIO1_IO00 0x40)?
Thank you in advance!