configure SAI3 output clock frequency in imx8mm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

configure SAI3 output clock frequency in imx8mm

6,411 Views
xcyhere
Contributor I

你好:

         我现在需要配置imx8mm的sai3 mclk时钟频率,让他输出i2s_mclk提供给外部audio codec(I2S slave mode),让audio codec的采样率为44.1kHz。而audio codec要想配置44.1kHz的采样率,他需要的mclk时钟只能选择:22579200 Hz、33868800 Hz、24000000 Hz,但是在配置设备树时候,发现他只支持2457600这一种频率(0误差),其他配置都会出现不同程度的误差:

pastedImage_1.png

出现误差导致在arecord命令执行时,调用fsl_sai_set_bclk()函数生成bclk时,出现无法分频的频率而异常退出结束:

pastedImage_2.png

请问这个问题怎么解决呢?

0 Kudos
Reply
7 Replies

6,188 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi xcy,

    i.mx8mm's clock driver is drivers/clk/imx/clk-imx8mm.c, open the file, you will see audio pll settings, like below:

static const struct imx_int_pll_rate_table imx8mm_audiopll_tbl[] = {

    PLL_1443X_RATE(786432000U, 262, 2, 2, 9437),
    PLL_1443X_RATE(722534400U, 361, 3, 2, 17511),
};

786432000 / 24576000 = 32

722534400 / 22579200 = 32

So you can change sai3 node like below:

&sai3 {
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_sai3>;
    assigned-clocks = <&clk IMX8MM_CLK_SAI3_SRC>,
            <&clk IMX8MM_CLK_SAI3_DIV>;
    assigned-clock-parents = <&clk IMX8MM_AUDIO_PLL2_OUT>;
    assigned-clock-rates = <0>, <22579200>;
    status = "okay";
};

Try it, please!

Have a nice day!

BR,

Weidong

0 Kudos
Reply

6,188 Views
xcyhere
Contributor I

hi Weidong,

      非常感谢你的回复,但是我还是不太明白,请教下:

   (1)当时我在追drivers/clk/imx/clk-imx8mm.c代码时,也想到修改audio时钟parent,但是在imx8mm手册中发现两者都是650MHz就没有改(722534400 和786432000 这两个频率含义不理解):

pastedImage_2.png

pastedImage_1.png

(2)为什么786432000 / 24576000 = 32和722534400 / 22579200 = 32,然后在设备树节点中修改assigned-clock-parents = <&clk IMX8MM_AUDIO_PLL2_OUT>;呢?

      IMX8MM_AUDIO_PLL1_OUT和IMX8MM_AUDIO_PLL2_OUT宏定义和32看不出联系是什么?

pastedImage_3.png

0 Kudos
Reply

6,188 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi

786432000和722534400,分别是配置PLL1和PLL2的输出频率,一个是24.576M的整数倍,一个是22.5792M的整数倍,那么当你需要48K的时候,用PLL1,44.1K的时候,用PLL2。

如果不是你时钟的整数倍,你怎么能去做整除分频呢?

伟东

0 Kudos
Reply

5,709 Views
bull-rider
Contributor I

你好!

我遇到和上面同样的问题,想要配置imx8qm的sai1 mclk时钟频率,让他输出i2s_mclk提供给外部audio codec(I2S slave mode),让audio codec的采样率为44.1kHz。

static int fsl_sai_set_bclk(struct snd_soc_dai *dai, bool tx, u32 freq)
{
struct fsl_sai *sai = snd_soc_dai_get_drvdata(dai);
unsigned char offset = sai->soc->reg_offset;
unsigned long clk_rate;
unsigned int reg = 0;
u32 ratio, savesub = freq, saveratio = 0, savediv = 0;
u32 id;
int ret = 0;

/* Don't apply to slave mode */
if (sai->slave_mode[tx])
return 0;

for (id = 0; id < FSL_SAI_MCLK_MAX; id++) {
clk_rate = clk_get_rate(sai->mclk_clk[id]);

if (!clk_rate)
continue;

ratio = clk_rate / freq;

ret = clk_rate - ratio * freq;
dev_err(dai->dev, "clk_rate: %ld freq: %d ret: %d\n",clk_rate,freq,ret);//无论播放什么格式的音频文件这里clk_rate=49152000

......

if (saveratio == 0) {
dev_err(dai->dev, "failed to derive required %cx rate: %d\n",//
tx ? 'T' : 'R', freq);
return -EINVAL;

....

}

设备树中sai1的配置

&sai1 {
#sound-dai-cells = <0>;
assigned-clocks = <&clk IMX_SC_R_AUDIO_PLL_0 IMX_SC_PM_CLK_PLL>,
<&clk IMX_SC_R_AUDIO_PLL_0 IMX_SC_PM_CLK_SLV_BUS>,
<&clk IMX_SC_R_AUDIO_PLL_0 IMX_SC_PM_CLK_MST_BUS>,
<&sai1_lpcg 0>; /* FIXME: should be sai1, original code is 0 */
assigned-clock-rates = <786432000>, <49152000>, <12288000>, <49152000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_sai1>;
status = "okay";
};

我这个要怎么修改?machine驱动使用的是simple-card.c.

问题出在哪里?

0 Kudos
Reply

5,309 Views
Ryze
Contributor I

你好,请问你解决了这个问题了吗?

0 Kudos
Reply

5,222 Views
bull-rider
Contributor I

这个问题已经解决了!

0 Kudos
Reply

4,888 Views
edwardtyrrell
Senior Contributor I

Hi,

I have the same problem could you share you soluion please?

Cheers.

0 Kudos
Reply