coexistence of wifi and bluetooth.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

coexistence of wifi and bluetooth.

1,253 次查看
mutyalaraoneela
Contributor III

Hi All,

Platform : imx6sl

Os : Android kitkat 4.4.3

     I made my module to run as wifi and bluetooth individually, but not I want to make it coexist. For that do I need to enable anything in the Android BSP????

Please suggest me how to proceed from here???

Thanks and Regards,

Mutyalarao.

0 项奖励
回复
1 回复

1,025 次查看
igorpadykov
NXP Employee
NXP Employee

Hi mutyalarao

bluetooth and wifi stacks need to speak to each other to know when

is an appropriate time to prefer wifi traffic or bluetooth traffic and AR6103

has special signals called Bluetooth Coexistence Interface, however these signals

are not routed on connector on Sabre board.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复