Hi Igor,
i also tried on pin GPIO1_IO03 (N5) muxed with CCM_CLKO2, it's pimnux and register dump is
fsl,pins = <
MX7D_PAD_GPIO1_IO03__CCM_CLKO2 0x00000014
>;
added in dts file,
root:~# /unit_tests/memtool -32 0x302C000C 4
E
Reading 0x4 count starting at address 0x302C000C
0x302C000C: 00000005 00000000 00000000 00000000
root:~#
i am not able to see any frequency on N5 ball point, i can change the mux configuration at runtime
to gpio by memtool and also can change the status of gpio but in CLKO2 mode i am not able to
make it functional.
in ALT5 mode this pin is at ground level only and not generating any frequency.
what seems to be the reason behind this issue.
regards,
Akash