clCreateKernelsInProgram

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

clCreateKernelsInProgram

2,805 Views
1019599657
Contributor III

Hi everyone,

I use opencl to detect object with yolo. And when i use API "clCreateKernelsInProgram" , i find it will stuck . 

My kernel num is 15. What can i do to solve it?

0 Kudos
Reply
3 Replies

2,733 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Li,

OpenCL is 2.1v and You have to use openCV 4.2, take in mind that in opencl 3.1v doesn´t have the Softmax function.

Regards

0 Kudos
Reply

2,733 Views
1019599657
Contributor III

Hi,

i use the version of opencl is 1.2v , and i dont use opencv.

And i fix the kernel api. When i run it with yolov3-tiny. it use about 170s.

Why it so slow? Is the reason of my code or GPU?

Thanks. 

0 Kudos
Reply

2,733 Views
1019599657
Contributor III

Hi everyone:

By testing one by one , i found that my kernel function "softmax" has some error , I cannot clCreatKernel it .And while i delete some line likes  "vstore16(localInput[i], 0, &x[i * 16]);" , it can create suceess ,How can you give me some help?

Thank very much.

Looking forward to your reply!

0 Kudos
Reply