cl-som-imx8 yocto - NXP BSP source repo sync failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

cl-som-imx8 yocto - NXP BSP source repo sync failure

2,366件の閲覧回数
ecsatya
Contributor I

Hi,

I need to use the yocto build for cl-som-mx8 board and trying to sync the repo;

i'm following the instructions given @ https://github.com/compulab-yokneam/meta-compulab-imx8/wiki/01.-Build-CompuLab-Images

The repo sync is failing

> repo sync
Fetching project meta-fsl-bsp-release
Fetching project meta-openembedded
Fetching project meta-qt5
Fetching projects:  22% (2/9)  Fetching project meta-browser
Fetching projects:  33% (3/9)  Fetching project meta-freescale-distro
Fetching projects:  44% (4/9)  Fetching project poky
Fetching projects:  55% (5/9)  Fetching project meta-freescale-3rdparty
fatal: repository 'http://git.yoctoproject.org/poky/' not found
Fetching projects:  66% (6/9)  Fetching project fsl-community-bsp-base
Fetching projects:  77% (7/9)  Fetching project meta-freescale
fatal: repository 'http://git.yoctoproject.org/meta-freescale/' not found
fatal: repository 'http://git.yoctoproject.org/meta-freescale/' not found
fatal: repository 'http://git.yoctoproject.org/poky/' not found
error: Cannot fetch meta-freescale
error: Cannot fetch poky

error: Exited sync due to fetch errors

i'm behind a corporate firewall, and from some discussion thread i gather that certain proxy settings and port number are needed to access the git;

Kindly help me regarding the same

I'm also attaching the manifest file

Thanks

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,736件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satya

please check suggestions for firewall on link

OpenEmbedded 

also problems with compulab repositories can be posted on meta-fsl-arm mailing list

meta-freescale Info Page 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,736件の閲覧回数
ecsatya
Contributor I

Thanks igor,

my query was about repo sync of yocto github behind firewall; 

best regards

0 件の賞賛
返信