chown problem on yocto recipe db_6.0.30

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

chown problem on yocto recipe db_6.0.30

Jump to solution
5,766 Views
LPs
Contributor III

Hi all,

   I downloaded fsl-release-bsp 3.14 patch from repo.

I'm trying to bild core-image-minimal, but the process do_install of db_6..30.bb recipe because of the recipe try to chown directories.

The process stops and gives me hundreds of errors that chown fails to change permissions.

The error, as far as I know, is correct because of bitbake has to be launched as normal user, not as root. Then chown cannot be performed.

Am I missing something???

Labels (3)
Tags (2)
1 Solution
4,503 Views
LPs
Contributor III

At the end it was permission on ..../sources/poky/meta/bitbake/bin files and ..../sources/poky/scripts.

I don't know why, but all files was downloaded from repo with r--r--r-- permission.

View solution in original post

6 Replies
4,503 Views
ajithpv
Contributor V

Hi LPs​,

Could you please change the typo "chwon" to chown in your heading? This will helpful for other users to reach your post while searching in the community.

Cheers,

Ajith P V

0 Kudos
Reply
4,503 Views
LPs
Contributor III

I edited.

4,504 Views
LPs
Contributor III

At the end it was permission on ..../sources/poky/meta/bitbake/bin files and ..../sources/poky/scripts.

I don't know why, but all files was downloaded from repo with r--r--r-- permission.

4,503 Views
gusarambula
NXP TechSupport
NXP TechSupport

Thanks for updating on this issue. I’m sure it will help other community users.

I’ve also seen this happened to some other people but I don’t know the root cause. I think they just used chown over the whole BSP directory.

chown -R user.user fsl-release-bsp

0 Kudos
Reply
4,503 Views
vishnukumar
Contributor I

Its better to user userid instead of username,

chown -R 1000:1000 /path

0 Kudos
Reply
4,503 Views
LPs
Contributor III

I don't know the real cause. I importend sources dir from a pre setup svn repository created on a remote server.

Maybe something that belongs to users from different computers.

0 Kudos
Reply