changes in uboot(yocto) source are not reflecting on board(apalis-imx6q)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

changes in uboot(yocto) source are not reflecting on board(apalis-imx6q)

Jump to solution
1,524 Views
sumish_ks
Contributor II

Hi community,

i am trying to test a change in uboot that in uboot source file(apalis_imx6q.c) when i removed "sd-card" configuration and after that i have compiled(without error) it, i noticed that my board is getting boot properly so i just wanted to ask why this changes are not reflecting back on the board and  i am just trying to learn that if i wanted to do some changes in uboot then how it will be that is why i did this. please let me know if i have do some more additional changes or does it take any default configuration.

Thanks & best regards

Sumish

1 Solution
1,444 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sumish

one can check Chapter1 Porting U-Boot attached Porting Guide.

Also may be useful to ask support from vendor apalis board, toradex

Toradex - Customer Support 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,445 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sumish

one can check Chapter1 Porting U-Boot attached Porting Guide.

Also may be useful to ask support from vendor apalis board, toradex

Toradex - Customer Support 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply