cfimager windows 10 issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cfimager windows 10 issue

4,092 Views
shashikanthirem
Contributor III

cfimager.exe is not creating image properly in latest version of windows 10..please send me solution

Labels (3)
0 Kudos
Reply
4 Replies

3,822 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi shashikant,

Cfimager is not tested on windows 10, but which error are you seeing?

Regards

0 Kudos
Reply

3,531 Views
PowerTian
NXP Employee
NXP Employee
I occurred same issue when run cfimager with Win10, see error as below.
C:\Users\NXA16874\git\try_env\flow\bin>cfimager -raw -offset 0x400 -f gpu1_sd_image.bin -d D
Exception found: -22 Failed to locate scsi device
0 Kudos
Reply

3,822 Views
shashikanthirem
Contributor III

Hi, 

Any updates on the solutions? 

0 Kudos
Reply

3,822 Views
shashikanthirem
Contributor III

Hi,

Basically we are creating three partions for sdcard using cfimager for imx28 as follows :

1. VFAT partiton which contains firmware
2. Ext3 partiton for rootfs
3. another Ext3 partition for our rough work

The arguments for Creation of these patitons works well in windows 7 without any error and cfimager contains reformatting the drive for flashing files.

In windows 10 this is not happpening and error we are getting is as follows

Error -37 Failed to write sector

The above error we are getting while writing Extra data and to overcome this problem we formatted disk using diskpart and running cfimager works well.

Is There is a problem in windows or priveleged access in batch file/command prompt which is unknown for me.

Please let me know any solution.

0 Kudos
Reply