cannot enable systemd service

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

cannot enable systemd service

5,703件の閲覧回数
Egor_I_InertgasM
Contributor II

I have built Yocto Hardknott imx-5.10.35

https://github.com/varigit/variscite-bsp-platform.git -b fsl-hardknott -m imx-5.10.35-2.0.0-var01.xml

with MACHINE=imx8mp-var-dart DISTRO=fsl-imx-xwayland . var-setup-release.sh -b build_xwayland

image fsl-image-qt5

And I can not add service to autostart.

I write simple script

/opt/App/to_log.sh:

 

 

#!/bin/bash

echo log $(date) >> /opt/App/log.txt

 

 

And App_launcher.service is

 

 

[Unit]
Description=Start App application, restart by request, poweroff from application
#After=graphical.target
#After=weston.service

[Service]
Type=simple
ExecStart=/opt/App/to_log.sh
#ExecStart=/opt/App/App_launcher.sh

[Install]
WantedBy=multi-user.service

 

 

 

App_launcher.service in the /lib/systemd/system/ folder

Then I try to enable service:

 

 

~# sudo systemctl daemon-reload
[ 1249.464158] systemd-sysv-generator[1115]: SysV service '/etc/init.d/reboot' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 1249.488415] systemd-sysv-generator[1115]: SysV service '/etc/init.d/save-rtc.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
...(and other services)


~# cat /opt/App/log.txt

log Fri Aug 27 18:53:38 MSK 2021

~# sudo systemctl enable App_launcher
[ 1433.903998] systemd-sysv-generator[1142]: SysV service '/etc/init.d/reboot' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 1433.928120] systemd-sysv-generator[1142]: SysV service '/etc/init.d/save-rtc.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
...(and other services)

~# sudo systemctl status App_launcher
* App.service - Start App application, restart by request, poweroff from application
     Loaded: loaded (/lib/systemd/system/App.service; enabled; vendor preset: disabled)
     Active: inactive (dead)

Aug 27 18:35:48 imx8mp-var-dart systemd[1]: App.service: Succeeded.

 

 

Status is

(... vendor preset: disabled)
Active: inactive (dead)

And I can not set vendor preset to enabled.

After the reboot application does not starts, log.txt does not change.

How can autostart an application?

ラベル(3)
タグ(2)
0 件の賞賛
返信
1 返信

4,039件の閲覧回数
meetalipatel
Contributor III

Any updates on this issue? I am facing a similar issue.

0 件の賞賛
返信