can we port android on linux on I.MX6 board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

can we port android on linux on I.MX6 board

864 次查看
shalinikp
Contributor II

can we port android on linux on I.MX6 board ?

标签 (3)
0 项奖励
回复
2 回复数

755 次查看
Yuri
NXP Employee
NXP Employee

  Sorry, we do not have special notes about Android porting.

Nevertheless, hope the following helps.

Port Android to custom board


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

755 次查看
igorpadykov
NXP Employee
NXP Employee

Hi shalini

please check below ready Freescale Android releases (they are based on Linux),

may be they will suit.

Operating System Software-Board Support Packages (33)

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

Best regards

igor

0 项奖励
回复