can't specify ldb parameters on 3.10.53 kernel cmdline

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

can't specify ldb parameters on 3.10.53 kernel cmdline

1,898 次查看
chris_c
Contributor II

The 3.10.53 ldb driver appears to have been changed to support device tree nodes.  Does this mean there is no longer a way to specify ldb/timings on the command line?  This is pretty limiting if your device has several configurations (split mode ldb, versus single lvds channel, with different resolutions).   Any ideas on how to use device tree to achieve the same thing?

0 项奖励
回复
3 回复数

1,389 次查看
chris_c
Contributor II

But can you specify whether to use split mode/single channel dynamically in the bootargs?

0 项奖励
回复

1,389 次查看
BiyongSUN
NXP Employee
NXP Employee

Please check the ldb binding guide for device tree

Documentation/devicetree/bindings/video/fsl,ldb.txt

24 Optional properties:

25 - ext-ref: Provide this bool property if your LDB uses an external

26   reference resistor for bandgap.

27 - split-mode: Provide this bool property if your board uses LDB split

28   mode to drive a high resolution display, say 1080P@60.  In this

29   mode, two LVDS channels will drive one display.

30 - dual-mode: Provide this bool property if your board uses LDB dual

31   mode to drive two displays.  In this mode, one display engine will

32   drive two displays which have the same timings and display content.

display timing is part of linux.

0 项奖励
回复

1,389 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Regarding the timing parameters, you can use ranges in the device node.

Example:

        timing1: timing {

                /* 1920x1080p24 */

                clock-frequency = <148500000>;

                hactive = <1920>;

                vactive = <1080>;

                hsync-len = <0 44 60>;

                hfront-porch = <80 88 95>;

                hback-porch = <100 148 160>;

                vfront-porch = <0 4 6>;

                vback-porch = <0 36 50>;

                vsync-len = <0 5 6>;

        };

But you can still specify some parameters and display configuration in the bootargs.

For exmaple for LVDS and HDMI dual displays:

U-Boot > setenv displayinfo 'video=mxcfb1:dev=ldb video=mxcfb0:dev=hdmi,

1920x1080M@60,if=RGB24'

0 项奖励
回复