The 3.10.53 ldb driver appears to have been changed to support device tree nodes. Does this mean there is no longer a way to specify ldb/timings on the command line? This is pretty limiting if your device has several configurations (split mode ldb, versus single lvds channel, with different resolutions). Any ideas on how to use device tree to achieve the same thing?
Please check the ldb binding guide for device tree
Documentation/devicetree/bindings/video/fsl,ldb.txt
24 Optional properties:
25 - ext-ref: Provide this bool property if your LDB uses an external
26 reference resistor for bandgap.
27 - split-mode: Provide this bool property if your board uses LDB split
28 mode to drive a high resolution display, say 1080P@60. In this
29 mode, two LVDS channels will drive one display.
30 - dual-mode: Provide this bool property if your board uses LDB dual
31 mode to drive two displays. In this mode, one display engine will
32 drive two displays which have the same timings and display content.
display timing is part of linux.
Hi,
Regarding the timing parameters, you can use ranges in the device node.
Example:
timing1: timing {
/* 1920x1080p24 */
clock-frequency = <148500000>;
hactive = <1920>;
vactive = <1080>;
hsync-len = <0 44 60>;
hfront-porch = <80 88 95>;
hback-porch = <100 148 160>;
vfront-porch = <0 4 6>;
vback-porch = <0 36 50>;
vsync-len = <0 5 6>;
};
But you can still specify some parameters and display configuration in the bootargs.
For exmaple for LVDS and HDMI dual displays:
U-Boot > setenv displayinfo 'video=mxcfb1:dev=ldb video=mxcfb0:dev=hdmi,
1920x1080M@60,if=RGB24'