can't boot emmc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
11,424件の閲覧回数
ningli
Contributor III

hi,

i am using imx6sl custom boad and android4.4, i find a problem and don't know how to deal it .

can anyone give me some s guid?

filesystem can not mount sucessful!  look the log, emmc write timeout ! why? thanks everyone!

U-Boot 2009.08-dirty ( 4鏈26 2016 - 10:17:15)

U-Boot code: 87800640 -> 87833000  BSS: -> 8786DC30

CPU: Freescale i.MX6 family TO1.2 at 396 MHz

Thermal sensor with ratio = 185

Temperature:   41 C, calibration data 0x5945175f

mx6q pll1: 792MHz

mx6q pll2: 528MHz

mx6q pll3: 480MHz

mx6q pll8: 50MHz

ipg clock     : 49500000Hz

ipg per clock : 49500000Hz

uart clock    : 80000000Hz

cspi clock    : 60000000Hz

ahb clock     : 99000000Hz

axi clock   : 198000000Hz

emi_slow clock: 99000000Hz

ddr clock     : 396000000Hz

usdhc1 clock  : 198000000Hz

usdhc2 clock  : 198000000Hz

usdhc3 clock  : 198000000Hz

usdhc4 clock  : 198000000Hz

Board: MX6SoloLite-EVK (0x60312): [ POR ]

Boot Device: MMC

I2C:   ready

RAM Configuration:

Bank #0: 80000000  1.2 GB

MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2

In:    serial

Out:   serial

Err:   serial

Found PFUZE100! deviceid=10,revid=21

Net:   got MAC address from IIM: 00:00:00:00:00:00

FEC0 [PRIME]

### main_loop entered: bootdelay=3

### main_loop: bootcmd="booti mmc0"

Hit any key to stop autoboot:  0

lining debug abortboot return abort =  0

ptn 0 name='boot' start=53248 len=27262976

booti: mmc read kernel pte->start = 0x0000d000

booti: mmc read kernel hdr->page_size = 2048

booti: mmc read kernel mmcc = 0

booti: mmc read kernel sector = 0x0000d004

booti: mmc read kernel (hdr->kernel_size / 512) + 1 = 9324

booti: mmc read kernel (void *)hdr->kernel_addr = 0x80800000

   Image magic:   ANDROID!

                          譎

   kernel_size:   0x48d70c

   kernel_addr:   0x80800000

   rdisk_size:   0x79b0d

   rdisk_addr:   0x81800000

   second_size:   0x0

   second_addr:   0x81700000

   tags_addr:   0x80800100

   page_size:   0x800

   name:     

   cmdline:   console=ttymxc0,115200 init=/init tps65185:pass=2,vcom=-2030000 video=mxcepdcfb:E97_V110,bpp=16 androidboot.console=ttymxc0 video=mxc_elcdif_fb:off androidboot.hardware=freescale2020000

   id[0]:   0x0

   id[1]:   0x0

   id[2]:   0x0

   id[3]:   0x0

   id[4]:   0x0

   id[5]:   0x0

   id[6]:   0x0

   id[7]:   0x0

kernel   @ 80800000 (4773644)

ramdisk  @ 81800000 (498445)

kernel cmdline:

        use boot.img command line:

        console=ttymxc0,115200 init=/init tps65185:pass=2,vcom=-2030000 video=mxcepdcfb:E97_V110,bpp=16 androidboot.console=ttymxc0 video=mxc_elcdif_fb:off androidboot.hardware=freescale androidboot.serialno=0b27b1d4df669563

params->u.mem.start = 0x80000000

params->u.mem.size = 0x7fffffff

Starting kernel ...

Initializing cgroup subsys cpuset

Initializing cgroup subsys cpu

Linux version 3.0.35-06532-gdfe90de-dirty (root@HP-Z230-Workstation) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #151 PREEMPT Thu Jun 23 18:02:09 CST 2016

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX 6SoloLite EVK Board

Memory policy: ECC disabled, Data cache writeback

CPU identified as i.MX6SoloLite, silicon rev 1.2

On node 0 totalpages: 511999

free_area_init_node: node 0, pgdat c0cb0d04, node_mem_map c187a000

  Normal zone: 1344 pages used for memmap

  Normal zone: 0 pages reserved

  Normal zone: 170688 pages, LIFO batch:31

  HighMem zone: 2752 pages used for memmap

  HighMem zone: 337215 pages, LIFO batch:31

pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768

pcpu-alloc: [0] 0

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 507903

Kernel command line: console=ttymxc0,115200 init=/init tps65185:pass=2,vcom=-2030000 video=mxcepdcfb:E97_V110,bpp=16 androidboot.console=ttymxc0 video=mxc_elcdif_fb:off androidboot.hardware=freescale androidboot.serialno=0b27b1d4df669563

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 1999MB = 1999MB total

Memory: 2016064k/2016064k available, 81084k reserved, 1359868K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    DMA     : 0xfbe00000 - 0xffe00000   (  64 MB)

    vmalloc : 0xea800000 - 0xf2000000   ( 120 MB)

    lowmem  : 0xc0000000 - 0xea000000   ( 672 MB)

    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

    modules : 0xbf000000 - 0xbfe00000   (  14 MB)

      .init : 0xc0008000 - 0xc0038000   ( 192 kB)

      .text : 0xc0038000 - 0xc0c4c668   (12370 kB)

      .data : 0xc0c4e000 - 0xc0cb18c0   ( 399 kB)

       .bss : 0xc0cb18e4 - 0xc0ddea48   (1205 kB)

Preemptible hierarchical RCU implementation.

NR_IRQS:624

MXC GPIO hardware

sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956ms

*************reg:0xc0011740*********

arm_max_freq=1GHz

MXC_Early serial console at MMIO 0x2020000 (options '115200')

bootconsole [ttymxc0] enabled

Calibrating delay loop... 789.70 BogoMIPS (lpj=3948544)

pid_max: default: 32768 minimum: 301

Security Framework initialized

Mount-cache hash table entries: 512

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

do_kern_mount1

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

do_kern_mount3

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 2

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

CPU: Testing write buffer coherency: ok

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

NET: Registered protocol family 16

->drivers/i2c/i2c-boardinfo.c:i2c_register_board_info :0

->bus_num 0:0 rt9428:0x36

->bus_num 0:1 tps65185:0x68

->drivers/i2c/i2c-boardinfo.c:i2c_register_board_info :1

->drivers/i2c/i2c-boardinfo.c:i2c_register_board_info :2

->drivers/i2c/i2c-boardinfo.c:i2c_register_board_info :3

->bus_num 0:0 pfuze100:0x8

hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.

hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.

hw-breakpoint: maximum watchpoint size is 4 bytes.

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32030000, Cache size: 262144 B

bio: create slab <bio-0> at 0

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

Freescale USB OTG Driver loaded, $Revision: 1.55 $

mc_pfuze 0-0008: ID: 0,Full lay: 2 ,Metal lay: 1

mc_pfuze 0-0008: FAB: 0 ,FIN: 0

->pfuze100_init

->pfuze100 version:21

->pfuze100 VGEN1 CTL:18

->pfuze100 VGEN1 VOLT:0

->pfuze100 VGEN1 VOLT:0

->pfuze100 VGEN1 CTL:18

->pfuze100 init end

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Version 1.0.24.

NET: Registered protocol family 23

Bluetooth: Core ver 2.16

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

cfg80211: Calling CRDA to update world regulatory domain

-----------tps65185_probe---------

client->name = tps65185, client->addr = 0x68

i2c-core: driver [tps65185] using legacy suspend method

i2c-core: driver [tps65185] using legacy resume method

rt_fg_get_property: FG_SOC=1020, SYS_SOC=100

rt_fg_get_property: FG_SOC=1020, SYS_SOC=100

add wake up source irq 105

rt9428 0-0036: driver successfully loaded

i2c-core: driver [rt9428] using legacy suspend method

i2c-core: driver [rt9428] using legacy resume method

Switching to clocksource mxc_timer1

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

FS-Cache: Loaded

CacheFiles: Loaded

NET: Registered protocol family 2

IP route cache hash table entries: 32768 (order: 5, 131072 bytes)

TCP established hash table entries: 131072 (order: 8, 1048576 bytes)

TCP bind hash table entries: 65536 (order: 6, 262144 bytes)

TCP: Hash tables configured (established 131072 bind 65536)

TCP reno registered

UDP hash table entries: 512 (order: 1, 8192 bytes)

UDP-Lite hash table entries: 512 (order: 1, 8192 bytes)

/**************rt9428_dwork_func************/

/**************rt9428_update_info************/

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Unpacking initramfs...

rt9428_update_info: REG_CFG = 0x325f

rt9428_update_info: REG_STATUS = 0x0000

rt9428_update_info: FG_VBAT = 4295

rt9428_update_info: ORG_TEMP = 31, TEMP = 25

rt9428_update_info: FG_SOC = 1020

rt9428_update_info: VG1 = 0x8132

Freeing initrd memory: 484K

etb: probe of etb failed with error -2

etm: probe of etm.0 failed with error -2

rt9428_update_info: VG2 = 0x8232

Static Power Management for Freescale i.MX6

wait mode is enabled for i.MX6

cpaddr = ea820000 suspend_iram_base=ea818000

PM driver module loaded

IMX usb wakeup probe

rt9428_update_info: VG3 = 0x8332

the wakeup pdata is 0xe616df60

add wake up source irq 75

rt9428_update_info: VG4 = 0x8332

IMX usb wakeup probe

the wakeup pdata is 0xe616dd60

rt9428_update_info: CVS = 0x8332

/**************rt9428_update_info**end**********/

cpu regulator mode:ldo_bypass

rt_fg_get_property: FG_SOC=1020, SYS_SOC=100

_regulator_get: get() with no identifier

mx6_cpu_regulator_init: failed to get pu regulator

i.MXC CPU frequency driver

audit: initializing netlink socket (disabled)

type=2000 audit(0.800:1): initialized

highmem bounce pool size: 64 pages

ashmem: initialized

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

NTFS driver 2.1.30 [Flags: R/O].

JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.

fuse init (API version 7.16)

msgmni has been set to 1282

NET: Registered protocol family 38

cryptodev: driver loaded.

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

imx-sdma imx-sdma: loaded firmware 1.1

imx-sdma imx-sdma: initialized

Serial: IMX driver

imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX

console [ttymxc0] enabled, bootconsole disabled

console [ttymxc0] enabled, bootconsole disabled

loop: module loaded

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

PPP generic driver version 2.4.2

PPP Deflate Compression module registered

PPP BSD Compression module registered

PPP MPPE Compression module registered

NET: Registered protocol family 24

RTL871X: module init start

RTL871X: rtl8189es v4.3.10_12447.20141008

RTL871X: build time: Jun 12 2016 10:31:48

RTL871X: module init ret=0

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1

fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000

fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00

usb usb1: usb_autoresume_device: cnt 5 -> 1

usb usb1: usb_autoresume_device: cnt 6 -> 1

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

usb usb1: usb_autosuspend_device: cnt 4 -> 0

usb usb1: usb_autosuspend_device: cnt 3 -> 0

add wake up source irq 74

fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2

fsl-ehci fsl-ehci.1: irq 74, io base 0x02184200

fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00

usb usb2: usb_autoresume_device: cnt 5 -> 1

usb usb2: usb_autoresume_device: cnt 6 -> 1

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

usb usb2: usb_autosuspend_device: cnt 4 -> 0

usb usb2: usb_autosuspend_device: cnt 3 -> 0

usbcore: registered new interface driver cdc_acm

hub 1-0:1.0: usb_autopm_put_interface_async: cnt 1 -> 0

hub 1-0:1.0: usb_autopm_get_interface: cnt 2 -> 1

cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters

Initializing USB Mass Storage driver...

hub 1-0:1.0: usb_autopm_put_interface: cnt 0 -> 0

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

usbcore: registered new interface driver usbserial

usbserial: USB Serial Driver core

USB Serial support registered for GSM modem (1-port)

usbcore: registered new interface driver option

option: v0.7.2:USB Driver for GSM modems

USB Serial support registered for Qualcomm USB modem

usbcore: registered new interface driver qcserial

ARC USBOTG Device Controller driver (1 August 2005)

imx6 usb charger online:0

android_usb gadget: Mass Storage Function, version: 2009/09/11

hub 2-0:1.0: usb_autopm_put_interface_async: cnt 1 -> 0

hub 2-0:1.0: usb_autopm_get_interface: cnt 2 -> 1

hub 2-0:1.0: usb_autopm_put_interface: cnt 0 -> 0

android_usb gadget: Number of LUNs=1

lun0: LUN: removable file: (no medium)

Gadget Android: controller 'fsl-usb2-udc' not recognized

android_usb gadget: android_usb ready

Suspend udc for OTG auto detect

USB Host suspend begins

will suspend roothub and its children

hub 1-0:1.0: usb_suspend_interface: status 0

ehci_fsl_bus_suspend begins, DR

ehci_fsl_bus_suspend ends, DR

usb usb1: usb_suspend_device: status 0

usb usb1: usb_suspend_both: status 0

host suspend ends

USB Gadget resume begins

fsl_udc_resume, Wait for wakeup thread finishes

dr_controller_run: udc out low power mode

USB Gadget resume ends

fsl-usb2-udc: bind to driver android_usb

input: imx-keypad as /devices/platform/imx-keypad/input/input0

-----code:102 val:0-----

-----code:114 val:0-----

-----code:115 val:0-----

-----code:105 val:0-----

-----code:106 val:0-----

add wake up source irq 103

----------pen probe-------------------

---uart clk is:80000000-----------

-----pen_tablet_init--------

-----pen_tablet_power----status = 0--

---------uart2 gpio init---------

-----pen_tablet_power----status = 1--

---------uart2 init---------

imx-uart.1: ttymxc1 at MMIO 0x2024000 (irq = 59) is a IMX

--------serial_8250_probe:612---------

--------serial_8250_startup:324---------

UCR1:0

UCR2:1

UCR3:700

UCR4:8000

UFCR:801

USR1:2040

USR2:4008

UBIR:0

UBMR:0

UBRC:4

UTS:60

--------serial_8250_startup:341---------

UCR1:1

UCR2:1

UCR3:700

UCR4:8000

UFCR:801

USR1:2040

USR2:4008

UBIR:0

UBMR:0

UBRC:4

UTS:60

--------serial_8250_startup:345---------

UCR1:1

UCR2:6027

UCR3:700

UCR4:8000

UFCR:801

USR1:2040

USR2:5008

UBIR:0

UBMR:0

UBRC:4

UTS:60

--------serial_8250_startup:349---------

UCR1:1

UCR2:6027

UCR3:700

UCR4:8000

UFCR:801

USR1:2040

USR2:5008

UBIR:0

UBMR:0

UBRC:4

UTS:60

--------serial_8250_startup:359---------

UCR1:1

UCR2:6027

UCR3:704

UCR4:8000

UFCR:801

USR1:2040

USR2:5008

UBIR:0

UBMR:0

UBRC:4

UTS:60

--------serial_8250_startup:371---------

UCR1:1

UCR2:6027

UCR3:704

UCR4:3810

UFCR:801

USR1:2040

USR2:5008

UBIR:0

UBMR:0

UBRC:4

UTS:60

--------serial_8250_startup:377---------

UCR1:1

UCR2:6027

UCR3:704

UCR4:3810

UFCR:1301

USR1:2040

USR2:5008

UBIR:0

UBMR:0

UBRC:4

UTS:60

--------serial_8250_startup:382---------

UCR1:1

UCR2:6027

UCR3:704

UCR4:3810

UFCR:1301

USR1:2040

USR2:5008

UBIR:bf

UBMR:0

UBRC:4

UTS:60

--------serial_8250_startup:386---------

UCR1:1

UCR2:6027

UCR3:704

UCR4:3810

UFCR:1301

USR1:2040

USR2:5008

UBIR:bf

UBMR:1be5

UBRC:4

UTS:60

--------serial_8250_startup:390---------

UCR1:601

UCR2:6027

UCR3:704

UCR4:3810

UFCR:1301

USR1:2040

USR2:5008

UBIR:bf

UBMR:1be5

UBRC:4

UTS:60

--------serial_8250_startup:394---------

--------serial_8250_probe:628---------

input: elan-touch as /devices/virtual/input/input1

fsl-usb2-udc fsl-usb2-udc: Plug Contact = 1

--------serial_8250_probe:650---------

Hanwon Serial tablet driver!

using rtc device, snvs_rtc, for alarms

snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0

i2c /dev entries driver

Linux video capture interface: v2.00

usbcore: registered new interface driver uvcvideo

USB Video Class driver (v1.1.0)

i2c-core: driver [mag3110] using legacy suspend method

i2c-core: driver [mag3110] using legacy resume method

fsl-usb2-udc fsl-usb2-udc: It is a stardard downstream port

charger is SDP

imx6 usb charger online:1

-----------tps65185_sensor_probe---------

imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)

device-mapper: uevent: version 1.0.3

device-mapper: ioctl: 4.20.0-ioctl (2011-02-02) initialised: [email protected]

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci [sdhci_add_host()]: Disabling ADMA as it is marked broken

sdhci [sdhci_add_host()]: mmc0: Auto-CMD23 unavailable

sdhci: =========== REGISTER DUMP (mmc0)===========

sdhci: Sys addr: 0x00000000 | Version:  0x00000202

sdhci: Blk size: 0x00000200 | Blk cnt:  0x00000001

sdhci: Argument: 0x00000000 | Trn mode: 0x00000000

sdhci: Present:  0xfff98088 | Host ctl: 0x00000020

sdhci: Power:    0x0000000d | Blk gap:  0x00000000

sdhci: Wake-up:  0x00000000 | Clock:    0x00000018

sdhci: Timeout:  0x00000000 | Int stat: 0x00000000

sdhci: Int enab: 0x007f0003 | Sig enab: 0x007f0003

sdhci: AC12 err: 0x00000000 | Slot int: 0x00000202

sdhci: Caps:     0x07ebb407 | Caps_1:   0x0000b407

sdhci: Cmd:      0x00000d1a | Max curr: 0x00ffffff

sdhci: Host ctl2: 0x00000000

sdhci: ===========================================

mmc0: clock 0Hz busmode 1 powermode 0 cs 0 Vdd 0 width 0 timing 0

mmc0: mmc_rescan_try_freq: trying to init card at 400000 Hz

mmc0: clock 0Hz busmode 1 powermode 1 cs 0 Vdd 21 width 0 timing 0

mmc0: SDHCI controller on platform [sdhci-esdhc-imx.0] using DMA

android_work: did not send uevent (0 0   (null))

Galcore version 4.6.9.9754

Thermal calibration data is 0x5945175f

mmc0: clock 400000Hz busmode 1 powermode 2 cs 0 Vdd 21 width 0 timing 0

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

Thermal sensor with ratio = 185

Anatop Thermal registered as thermal_zone0

anatop_thermal_probe: default cooling device is cpufreq!

mmc0: starting CMD52 arg 00000c00 flags 00000195

android_usb gadget: unknown class-specific control req 80.06 v0100 i0000 l64

USB Gadget resume begins

fsl_udc_resume, Wait for wakeup thread finishes

usbcore: registered new interface driver usbhid

android_work: sent uevent USB_STATE=CONNECTED

usbhid: USB HID core driver

android_work: sent uevent USB_STATE=DISCONNECTED

logger: created 256K log 'log_main'

logger: created 256K log 'log_events'

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req done (CMD52): -110: 00000000 00000000 00000000 00000000

mmc0: starting CMD52 arg 80000c08 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req done (CMD52): -110: 00000000 00000000 00000000 00000000

mmc0: clock 400000Hz busmode 1 powermode 2 cs 1 Vdd 21 width 0 timing 0

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

logger: created 256K log 'log_radio'

logger: created 256K log 'log_system'

usbcore: registered new interface driver snd-usb-audio

mmc0: starting CMD0 arg 00000000 flags 000000c0

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD0): 0: 00000000 00000000 00000000 00000000

mmc0: clock 400000Hz busmode 1 powermode 2 cs 0 Vdd 21 width 0 timing 0

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

android_usb gadget: unknown class-specific control req 80.06 v0100 i0000 l18

android_work: sent uevent USB_STATE=CONNECTED

android_usb gadget: unknown class-specific control req 80.06 v0200 i0000 l255

ALSA device list:

  No soundcards found.

u32 classifier

    Actions configured

Netfilter messages via NETLINK v0.30.

nf_conntrack version 0.5.0 (16384 buckets, 65536 max)

ctnetlink v0.93: registering with nfnetlink.

NF_TPROXY: Transparent proxy support initialized, version 4.1.0

NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.

mmc0: starting CMD8 arg 000001aa flags 000002f5

xt_time: kernel timezone is -0000

ip_tables: (C) 2000-2006 Netfilter Core Team

arp_tables: (C) 2002 David S. Miller

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req done (CMD8): -110: 00000000 00000000 00000000 00000000

mmc0: starting CMD5 arg 00000000 flags 000002e1

TCP cubic registered

Initializing XFRM netlink socket

NET: Registered protocol family 10

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req failed (CMD5): -110, retrying...

Mobile IPv6

ip6_tables: (C) 2000-2006 Netfilter Core Team

NET: Registered protocol family 17

NET: Registered protocol family 15

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req failed (CMD5): -110, retrying...

lib80211: common routines for IEEE802.11 drivers

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req failed (CMD5): -110, retrying...

lib80211_crypt: registered algorithm 'NULL'

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req done (CMD5): -110: 00000000 00000000 00000000 00000000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

lib80211_crypt: registered algorithm 'WEP'

lib80211_crypt: registered algorithm 'CCMP'

android_work: sent uevent USB_STATE=DISCONNECTED

lib80211_crypt: registered algorithm 'TKIP'

mmc0: starting CMD55 arg 00000000 flags 000000f5

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req done (CMD55): -110: 00000000 00000000 00000000 00000000

Bus freq driver module loaded

Bus freq driver Enabled

mxc_dvfs_core_probe

mmc0: starting CMD55 arg 00000000 flags 000000f5

DVFS driver module loaded

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

android_usb gadget: unknown class-specific control req 80.06 v0100 i0000 l64

mmc0: req done (CMD55): -110: 00000000 00000000 00000000 00000000

android_work: did not send uevent (0 0   (null))

mmc0: starting CMD55 arg 00000000 flags 000000f5

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req done (CMD55): -110: 00000000 00000000 00000000 00000000

mmc0: starting CMD55 arg 00000000 flags 000000f5

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req done (CMD55): -110: 00000000 00000000 00000000 00000000

mmc0: starting CMD1 arg 00000000 flags 000000e1

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD1): 0: 00ff8080 00000000 00000000 00000000

mmc0: clock 400000Hz busmode 1 powermode 2 cs 0 Vdd 7 width 0 timing 0

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

MXCFB_SET_WAVEFORM_MODES:4018462b

MXCFB_SET_TEMPERATURE:4004462c

MXCFB_SET_AUTO_UPDATE_MODE:4004462d

MXCFB_SEND_UPDATE:4040462e

MXCFB_WAIT_FOR_UPDATE_COMPLETE:c008462f

MXCFB_SET_PWRDOWN_DELAY:40044630

MXCFB_GET_PWRDOWN_DELAY:80044631

mmc0: clock 400000Hz busmode 1 powermode 2 cs 0 Vdd 7 width 0 timing 0

android_usb gadget: unknown class-specific control req 80.06 v0100 i0000 l18

MXCFB_SET_UPDATE_SCHEME:40044632

android_usb gadget: unknown class-specific control req 80.06 v0200 i0000 l255

android_work: sent uevent USB_STATE=CONNECTED

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

MXCFB_GET_WORK_BUFFER:c0044634

imx_epdc_fb imx_epdc_fb: ---resolution 1200x825, bpp 16

imx_epdc_fb imx_epdc_fb: ---xres: 1216, yres:896, max:1089536

imx_epdc_fb imx_epdc_fb: ---xres: 832, yres:1280, max:1064960

imx_epdc_fb imx_epdc_fb: ---buf_size allocate: 2179072, x_mem_size:0

mmc0: clock 400000Hz busmode 1 powermode 2 cs 1 Vdd 7 width 0 timing 0

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

imx_epdc_fb imx_epdc_fb: ---map_size allocate: 6537216, num_screen:3

imx_epdc_fb imx_epdc_fb: ---screen_base allocated at ff400000:0xff400000, 0xa6800000

mmc0: starting CMD0 arg 00000000 flags 000000c0

imx_epdc_fb imx_epdc_fb: ---EPDC version = 21

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD0): 0: 00000000 00000000 00000000 00000000

mmc0: clock 400000Hz busmode 1 powermode 2 cs 0 Vdd 7 width 0 timing 0

imx_epdc_fb imx_epdc_fb: ---upd_list[0]:0xe60019a0, size: 20

android_work: sent uevent USB_STATE=DISCONNECTED

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

imx_epdc_fb imx_epdc_fb: ---upd_list[1]:0xe60019e0, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[2]:0xe6001a00, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[3]:0xe6001a20, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[4]:0xe6001a40, size: 20

mmc0: starting CMD1 arg 40000080 flags 000000e1

imx_epdc_fb imx_epdc_fb: ---upd_list[5]:0xe60019c0, size: 20

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD1): 0: 00ff8080 00000000 00000000 00000000

imx_epdc_fb imx_epdc_fb: ---upd_list[6]:0xe60017c0, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[7]:0xe6001a60, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[8]:0xe6001a80, size: 20

android_usb gadget: unknown class-specific control req 80.06 v0100 i0000 l64

mmc0: starting CMD1 arg 40000080 flags 000000e1

imx_epdc_fb imx_epdc_fb: ---upd_list[9]:0xe6001ac0, size: 20

android_work: sent uevent USB_STATE=CONNECTED

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD1): 0: c0ff8080 00000000 00000000 00000000

mmc0: starting CMD2 arg 00000000 flags 00000067

imx_epdc_fb imx_epdc_fb: ---upd_list[10]:0xe6001b00, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[11]:0xe6001b20, size: 20

android_work: sent uevent USB_STATE=DISCONNECTED

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD2): 0: 11010030 30384737 300088b9 2cb94200

mmc0: starting CMD3 arg 00010000 flags 00000015

imx_epdc_fb imx_epdc_fb: ---upd_list[12]:0xe6001ae0, size: 20

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD3): 0: 00000500 00000000 00000000 00000000

mmc0: clock 400000Hz busmode 2 powermode 2 cs 0 Vdd 7 width 0 timing 0

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

imx_epdc_fb imx_epdc_fb: ---upd_list[13]:0xe6001aa0, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[14]:0xe6001b60, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[15]:0xe6001b40, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[16]:0xe6001b80, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[17]:0xe6001ba0, size: 20

android_usb gadget: unknown class-specific control req 80.06 v0100 i0000 l18

mmc0: starting CMD9 arg 00010000 flags 00000007

android_usb gadget: unknown class-specific control req 80.06 v0200 i0000 l255

android_work: sent uevent USB_STATE=CONNECTED

imx_epdc_fb imx_epdc_fb: ---upd_list[18]:0xe6001c00, size: 20

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD9): 0: d0270032 0f5903ff ffffffe7 86400000

mmc0: starting CMD7 arg 00010000 flags 00000015

imx_epdc_fb imx_epdc_fb: ---upd_list[19]:0xe6001c20, size: 20

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD7): 0: 00000700 00000000 00000000 00000000

mmc0: starting CMD8 arg 00000000 flags 000000b5

mmc0:     blksz 512 blocks 1 flags 00000200 tsac 150 ms nsac 0

imx_epdc_fb imx_epdc_fb: ---upd_list[20]:0xe6001c40, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[21]:0xe6001c60, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[22]:0xe6001be0, size: 20

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

imx_epdc_fb imx_epdc_fb: ---upd_list[23]:0xe6001bc0, size: 20

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a

sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6486200, transferred 0x079e00 bytes, next 0xa6500000

mmc0: req done (CMD8): 0: 00000900 00000000 00000000 00000000

mmc0:     512 bytes transferred: 0

---mmc_init_card--- 3!/n

mmc0: starting CMD6 arg 03b90101 flags 0000049d

imx_epdc_fb imx_epdc_fb: ---upd_list[24]:0xe6001c80, size: 20

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD6): 0: 00000800 00000000 00000000 00000000

mmc0: starting CMD13 arg 00010000 flags 00000195

imx_epdc_fb imx_epdc_fb: ---upd_list[25]:0xe6001ca0, size: 20

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000900 00000000 00000000 00000000

mmc0: clock 400000Hz busmode 2 powermode 2 cs 0 Vdd 7 width 0 timing 1

imx_epdc_fb imx_epdc_fb: ---upd_list[26]:0xe6001cc0, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[27]:0xe6001ce0, size: 20

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000

imx_epdc_fb imx_epdc_fb: ---upd_list[28]:0xe6001d00, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[29]:0xe6001d20, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[30]:0xe6001d40, size: 20

mmc0: clock 52000000Hz busmode 2 powermode 2 cs 0 Vdd 7 width 0 timing 1

sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000

sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000

sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000

sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000

imx_epdc_fb imx_epdc_fb: ---upd_list[31]:0xe6001d60, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[32]:0xe6001d80, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[33]:0xe6001da0, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[34]:0xe6001dc0, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[35]:0xe6001de0, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[36]:0xe6001e00, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[37]:0xe6001e20, size: 20

mmc0: starting CMD8 arg 00000000 flags 000000b5

mmc0:     blksz 512 blocks 1 flags 00000200 tsac 150 ms nsac 0

imx_epdc_fb imx_epdc_fb: ---upd_list[38]:0xe6001e40, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[39]:0xe6001e60, size: 20

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a

sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6486000, transferred 0x07a000 bytes, next 0xa6500000

mmc0: req done (CMD8): 0: 00000900 00000000 00000000 00000000

mmc0:     512 bytes transferred: 0

---mmc_select_powerclass--- !/n

mmc0: starting CMD6 arg 03bb0a01 flags 0000049d

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD6): 0: 00000800 00000000 00000000 00000000

mmc0: starting CMD13 arg 00010000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000900 00000000 00000000 00000000

imx_epdc_fb imx_epdc_fb: ---upd_list[40]:0xe6001e80, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[41]:0xe6001ea0, size: 20

---mmc_init_card--- 4!/n

mmc0: starting CMD6 arg 03b70201 flags 0000049d

imx_epdc_fb imx_epdc_fb: ---upd_list[42]:0xe6001ec0, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[43]:0xe6001ee0, size: 20

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD6): 0: 00000800 00000000 00000000 00000000

mmc0: starting CMD13 arg 00010000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000900 00000000 00000000 00000000

mmc0: clock 52000000Hz busmode 2 powermode 2 cs 0 Vdd 7 width 3 timing 1

sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000

sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000

sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000

imx_epdc_fb imx_epdc_fb: ---upd_list[44]:0xe6001f00, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[45]:0xe6001f20, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[46]:0xe6001f40, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[47]:0xe6001f60, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[48]:0xe6001f80, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[49]:0xe6001fa0, size: 20

mmc0: starting CMD8 arg 00000000 flags 000000b5

mmc0:     blksz 512 blocks 1 flags 00000200 tsac 150 ms nsac 0

imx_epdc_fb imx_epdc_fb: ---upd_list[50]:0xe6001fc0, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[51]:0xe6001fe0, size: 20

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a

sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6486000, transferred 0x07a000 bytes, next 0xa6500000

mmc0: req done (CMD8): 0: 00000900 00000000 00000000 00000000

mmc0:     512 bytes transferred: 0

mmc0: starting CMD8 arg 00000000 flags 000000b5

imx_epdc_fb imx_epdc_fb: ---upd_list[52]:0xe60081e0, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[53]:0xe6008200, size: 20

mmc0:     blksz 512 blocks 1 flags 00000200 tsac 150 ms nsac 0

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a

sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6486000, transferred 0x07a000 bytes, next 0xa6500000

mmc0: req done (CMD8): 0: 00000900 00000000 00000000 00000000

mmc0:     512 bytes transferred: 0

---mmc_select_powerclass--- !/n

mmc0: starting CMD6 arg 03bb0a01 flags 0000049d

imx_epdc_fb imx_epdc_fb: ---upd_list[54]:0xe6008220, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[55]:0xe6008240, size: 20

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD6): 0: 00000800 00000000 00000000 00000000

mmc0: starting CMD13 arg 00010000 flags 00000195

imx_epdc_fb imx_epdc_fb: ---upd_list[56]:0xe6008260, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[57]:0xe6008280, size: 20

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000900 00000000 00000000 00000000

---mmc_init_card--- 4!/n

mmc0: starting CMD6 arg 03b70601 flags 0000049d

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD6): 0: 00000800 00000000 00000000 00000000

mmc0: starting CMD13 arg 00010000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000900 00000000 00000000 00000000

mmc0: clock 52000000Hz busmode 2 powermode 2 cs 0 Vdd 7 width 3 timing 5

imx_epdc_fb imx_epdc_fb: ---upd_list[58]:0xe60082a0, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[59]:0xe60082c0, size: 20

sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000

sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000

sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000

imx_epdc_fb imx_epdc_fb: ---upd_list[60]:0xe60082e0, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[61]:0xe640c980, size: 20

imx_epdc_fb imx_epdc_fb: ---upd_list[62]:0xe640c960, size: 20

mmc0: clock 52000000Hz busmode 2 powermode 2 cs 0 Vdd 7 width 3 timing 5

sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000

sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000

sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000

imx_epdc_fb imx_epdc_fb: ---upd_list[63]:0xe6ffe940, size: 20

imx_epdc_fb imx_epdc_fb: ---size of void*:4, sizeof dma:4, max_num_buffers:2

imx_epdc_fb imx_epdc_fb: ---upd_buf0 virt:0xE6FFE920, phys:0xE6FFE900

imx_epdc_fb imx_epdc_fb: ---upd_buf allocated 1089536 bytes virt:0xE7000000, phys:0xA7000000, PHYS_OFFSET:80000000

mmc0: new high speed DDR MMC card at address 0001

imx_epdc_fb imx_epdc_fb: ---upd_buf allocated 1089536 bytes virt:0xE7200000, phys:0xA7200000, PHYS_OFFSET:80000000

mmcblk0: mmc0:0001 008G70 7.28 GiB

mmcblk0boot0: mmc0:0001 008G70 partition 1 4.00 MiB

imx_epdc_fb imx_epdc_fb: ---copy 0xFF100000,phys_copy:0xA7800000, working:0xFEF00000, working_phys0xa7600000,work size:1980000

mmcblk0boot1: mmc0:0001 008G70 partition 2 4.00 MiB

submit_bh 1

---mmc_blk_rw_rq_prep-- !

mmc0: starting CMD18 arg 00000000 flags 000000b5

mmc0:     blksz 512 blocks 8 flags 00000200 tsac 150 ms nsac 0

submit_bh 2

submit_bh 3

submit_bh 4

mmc0:     CMD12 arg 00000000 flags 0000049d

imx_epdc_fb imx_epdc_fb: --num_luts:64 -lut:0xE63FC1E0, size u32*: 4

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a

sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6500000, transferred 0x080000 bytes, next 0xa6580000

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD18): 0: 00000900 00000000 00000000 00000000

mmc0:     4096 bytes transferred: 0

mmc0:     (CMD12): 0: 00000b00 00000000 00000000 00000000

submit_bh 1

---mmc_blk_rw_rq_prep-- !

submit_bh 2

submit_bh 3

submit_bh 4

mmc0: starting CMD18 arg 0001e000 flags 000000b5

mmc0:     blksz 512 blocks 8 flags 00000200 tsac 150 ms nsac 0

mmc0:     CMD12 arg 00000000 flags 0000049d

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a

sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6e80000, transferred 0x080000 bytes, next 0xa6f00000

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD18): 0: 00000900 00000000 00000000 00000000

mmc0:     4096 bytes transferred: 0

mmc0:     (CMD12): 0: 00000b00 00000000 00000000 00000000

submit_bh 1

---mmc_blk_rw_rq_prep-- !

mmc0: starting CMD18 arg 0011e000 flags 000000b5

submit_bh 2

submit_bh 3

submit_bh 4

imx_epdc_fb imx_epdc_fb: ---lut_map:0xe63fc0e0

mmc0:     blksz 512 blocks 8 flags 00000200 tsac 150 ms nsac 0

mmc0:     CMD12 arg 00000000 flags 0000049d

-----tps65185_vcom_set_voltage---

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a

sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6500000, transferred 0x080000 bytes, next 0xa6580000

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD18): 0: 00000900 00000000 00000000 00000000

mmc0:     4096 bytes transferred: 0

mmc0:     (CMD12): 0: 00000b00 00000000 00000000 00000000

usb usb1: usb_suspend_both: status 0

hub 2-0:1.0: usb_suspend_interface: status 0

ehci_fsl_bus_suspend begins, Host 1

submit_bh 1

submit_bh 2

submit_bh 3

---mmc_blk_rw_rq_prep-- !

submit_bh 4

mmc0: starting CMD18 arg 0021e000 flags 000000b5

mmc0:     blksz 512 blocks 8 flags 00000200 tsac 150 ms nsac 0

mmc0:     CMD12 arg 00000000 flags 0000049d

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a

sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6500000, transferred 0x080000 bytes, next 0xa6580000

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD18): 0: 00000900 00000000 00000000 00000000

mmc0:     4096 bytes transferred: 0

mmc0:     (CMD12): 0: 00000b00 00000000 00000000 00000000

submit_bh 1

---mmc_blk_rw_rq_prep-- !

mmc0: starting CMD18 arg 00222000 flags 000000b5

mmc0:     blksz 512 blocks 8 flags 00000200 tsac 150 ms nsac 0

submit_bh 2

submit_bh 3

submit_bh 4

ehci_fsl_bus_suspend ends, Host 1

usb usb2: usb_suspend_device: status 0

usb usb2: usb_suspend_both: status 0

mmc0:     CMD12 arg 00000000 flags 0000049d

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a

sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6e80000, transferred 0x080000 bytes, next 0xa6f00000

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD18): 0: 00000900 00000000 00000000 00000000

mmc0:     4096 bytes transferred: 0

mmc0:     (CMD12): 0: 00000b00 00000000 00000000 00000000

mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4

mmcblk0: p4 size 13017088 extends beyond EOD, truncated

submit_bh 1

---mmc_blk_part_switch--- !

mmc_switch part_config = 74; part_time = 100

mmc0: starting CMD6 arg 03b34a01 flags 0000049d

submit_bh 2

submit_bh 3

submit_bh 4

tps65185 0-0068: Vcom set : -1400 mV

-----tps65185_vcom_is_enabled---

-----tps65185_display_is_enable---

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD6): 0: 00000800 00000000 00000000 00000000

mmc0: starting CMD13 arg 00010000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000900 00000000 00000000 00000000

---mmc_blk_rw_rq_prep-- !

mmc0: starting CMD18 arg 00000000 flags 000000b5

regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on

mmc0:     blksz 512 blocks 8 flags 00000200 tsac 150 ms nsac 0

mmc0:     CMD12 arg 00000000 flags 0000049d

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a

sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa7500000, transferred 0x080000 bytes, next 0xa7580000

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD18): 0: 00000900 00000000 00000000 00000000

mmc0:     4096 bytes transferred: 0

mmc0:     (CMD12): 0: 00000b00 00000000 00000000 00000000

submit_bh 1

submit_bh 2

submit_bh 3

submit_bh 4

---mmc_blk_rw_rq_prep-- !

regulator_init_complete: PFUZE100_VGEN5: incomplete constraints, leaving on

mmc0: starting CMD18 arg 00000018 flags 000000b5

mmc0:     blksz 512 blocks 8 flags 00000200 tsac 150 ms nsac 0

mmc0:     CMD12 arg 00000000 flags 0000049d

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a

sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa7500000, transferred 0x080000 bytes, next 0xa7580000

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD18): 0: 00000900 00000000 00000000 00000000

mmc0:     4096 bytes transferred: 0

mmc0:     (CMD12): 0: 00000b00 00000000 00000000 00000000

mmcblk0boot1: unknown partition table

regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on

submit_bh 1

---mmc_blk_part_switch--- !

submit_bh 2

submit_bh 3

submit_bh 4

mmc_switch part_config = 73; part_time = 100

mmc0: starting CMD6 arg 03b34901 flags 0000049d

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD6): 0: 00000800 00000000 00000000 00000000

regulator_init_complete: SPKVDD: incomplete constraints, leaving on

mmc0: starting CMD13 arg 00010000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000900 00000000 00000000 00000000

---mmc_blk_rw_rq_prep-- !

mmc0: starting CMD18 arg 00000000 flags 000000b5

snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 08:20:13 UTC (30013)

mmc0:     blksz 512 blocks 8 flags 00000200 tsac 150 ms nsac 0

mmc0:     CMD12 arg 00000000 flags 0000049d

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a

sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa7400000, transferred 0x080000 bytes, next 0xa7480000

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD18): 0: 00000900 00000000 00000000 00000000

mmc0:     4096 bytes transferred: 0

mmc0:     (CMD12): 0: 00000b00 00000000 00000000 00000000

submit_bh 1

---mmc_blk_rw_rq_prep-- !

submit_bh 2

submit_bh 3

submit_bh 4

mmc0: starting CMD18 arg 00000018 flags 000000b5

mmc0:     blksz 512 blocks 8 flags 00000200 tsac 150 ms nsac 0

Freeing init memory: 192K

do_mount 1

do_mount 2

do_mount 3

do_mount 4

do_mount 5

do_mount 6

do_new_mount 1 type = tmpfs,flags = 0,mnt_flags = 33, name = tmpfs

mmc0:     CMD12 arg 00000000 flags 0000049d

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a

sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6580000, transferred 0x080000 bytes, next 0xa6600000

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD18): 0: 00000900 00000000 00000000 00000000

mmc0:     4096 bytes transferred: 0

mmc0:     (CMD12): 0: 00000b00 00000000 00000000 00000000

do_new_mount 2

do_new_mount 3

do_kern_mount1

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 2

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

do_kern_mount3

do_new_mount 4

do_new_mount 5 err = 0

do_mount 11 retval = 0

do_mount 1

do_mount 2

do_mount 3

do_mount 4

do_mount 5

do_mount 6

do_new_mount 1 type = devpts,flags = 0,mnt_flags = 32, name = devpts

mmcblk0boot0: unknown partition table

do_new_mount 2

do_new_mount 3

do_kern_mount1

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

do_kern_mount3

do_new_mount 4

do_new_mount 5 err = 0

do_mount 11 retval = 0

do_mount 1

do_mount 2

do_mount 3

do_mount 4

do_mount 5

do_mount 6

do_new_mount 1 type = proc,flags = 0,mnt_flags = 32, name = proc

do_new_mount 2

do_new_mount 3

do_kern_mount1

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

do_kern_mount3

do_new_mount 4

do_new_mount 5 err = 0

do_mount 11 retval = 0

do_mount 1

do_mount 2

do_mount 3

do_mount 4

do_mount 5

do_mount 6

do_new_mount 1 type = sysfs,flags = 0,mnt_flags = 32, name = sysfs

do_new_mount 2

do_new_mount 3

do_kern_mount1

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

do_kern_mount3

do_new_mount 4

do_new_mount 5 err = 0

do_mount 11 retval = 0

init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.

rt_fg_get_property: FG_SOC=1020, SYS_SOC=100

init: /dev/hw_random not found

keychord: using input dev imx-keypad for fevent

do_mount 1

do_mount 2

do_mount 3

do_mount 4

do_mount 5

do_mount 6

do_new_mount 1 type = cgroup,flags = 0,mnt_flags = 32, name = none

do_new_mount 2

do_new_mount 3

do_kern_mount1

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 2

mount_fs 3

mount_fs 10

mount_fs 11

vfs_kern_mount 4

do_kern_mount3

do_mount 11 retval = -2

do_mount 1

do_mount 2

do_mount 3

do_mount 4

do_mount 5

do_mount 6

do_new_mount 1 type = tmpfs,flags = 0,mnt_flags = 32, name = none

do_new_mount 2

do_new_mount 3

do_kern_mount1

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 2

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

do_kern_mount3

do_new_mount 4

do_new_mount 5 err = 0

do_mount 11 retval = 0

do_mount 1

do_mount 2

do_mount 3

do_mount 4

do_mount 5

do_mount 6

do_new_mount 1 type = cgroup,flags = 0,mnt_flags = 32, name = none

do_new_mount 2

do_new_mount 3

do_kern_mount1

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 2

mount_fs 3

mount_fs 10

mount_fs 11

vfs_kern_mount 4

do_kern_mount3

do_mount 11 retval = -2

do_mount 1

do_mount 2

do_mount 3

do_mount 4

do_mount 5

do_mount 6

do_new_mount 1 type = tmpfs,flags = 0,mnt_flags = 32, name = tmpfs

do_new_mount 2

do_new_mount 3

do_kern_mount1

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 2

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

do_kern_mount3

do_new_mount 4

do_new_mount 5 err = 0

do_mount 11 retval = 0

do_mount 1

do_mount 2

do_mount 3

do_mount 4

do_mount 5

do_mount 6

do_new_mount 1 type = tmpfs,flags = 0,mnt_flags = 32, name = tmpfs

do_new_mount 2

do_new_mount 3

do_kern_mount1

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 2

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

do_kern_mount3

do_new_mount 4

do_new_mount 5 err = 0

do_mount 11 retval = 0

do_mount 1

do_mount 2

do_mount 3

do_mount 4

do_mount 5

do_mount 6

do_new_mount 1 type = tmpfs,flags = 0,mnt_flags = 32, name = tmpfs

do_new_mount 2

do_new_mount 3

do_kern_mount1

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 2

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

do_kern_mount3

do_new_mount 4

do_new_mount 5 err = 0

do_mount 11 retval = 0

do_mount 1

do_mount 2

do_mount 3

do_mount 4

do_mount 5

do_mount 6

do_new_mount 1 type = tmpfs,flags = 0,mnt_flags = 32, name = tmpfs

do_new_mount 2

do_new_mount 3

do_kern_mount1

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 2

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

do_kern_mount3

do_new_mount 4

do_new_mount 5 err = 0

do_mount 11 retval = 0

do_mount 1

do_mount 2

do_mount 3

do_mount 4

do_mount 5

do_mount 6

do_new_mount 1 type = cgroup,flags = 0,mnt_flags = 32, name = none

do_new_mount 2

do_new_mount 3

do_kern_mount1

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 2

mount_fs 3

mount_fs 4

mount_fs 5

mount_fs 6

mount_fs 7

mount_fs 8

vfs_kern_mount 5

do_kern_mount3

do_new_mount 4

do_new_mount 5 err = 0

do_mount 11 retval = 0

do_mount 1

do_mount 2

do_mount 3

do_mount 4

do_mount 5

do_mount 6

do_new_mount 1 type = ext4,flags = 0,mnt_flags = 32, name = /dev/block/mmcblk0p5

do_new_mount 2

do_new_mount 3

do_kern_mount1

vfs_kern_mount 1

vfs_kern_mount 2

vfs_kern_mount 3

mount_fs 1

mount_fs 3

ext4_mount

mount_bdev 1

mount_bdev 2

mount_bdev 3

mount_bdev 4

mount_bdev 6

ext4_fill_super 1

ext4_fill_super 2

ext4_fill_super 3

ext4_fill_super 4

ext4_fill_super 5

ext4_fill_super 7

ext4_fill_super 7.1 

__bread block =400; size = 1

__getblk 1

__find_get_block 1

__find_get_block 3

__find_get_block 2

__getblk_slow 1

__find_get_block 1

__find_get_block 3

__find_get_block 2

__getblk_slow 2

__getblk_slow 3

__find_get_block 1

__find_get_block 3

__find_get_block 4

__find_get_block 2

__getblk 2

__bread 2

__bread_slow 1

__bread_slow 3

submit_bh 1

---mmc_blk_part_switch--- !

mmc_switch part_config = 72; part_time = 100

mmc0: starting CMD6 arg 03b34801 flags 0000049d

submit_bh 2

submit_bh 3

submit_bh 4

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req failed (CMD6): -110, retrying...

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req failed (CMD6): -110, retrying...

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req failed (CMD6): -110, retrying...

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req done (CMD6): -110: 00000000 00000000 00000000 00000000

---mmc_blk_part_switch--- !

mmc_switch part_config = 72; part_time = 100

mmc0: starting CMD6 arg 03b34801 flags 0000049d

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req failed (CMD6): -110, retrying...

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req failed (CMD6): -110, retrying...

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req failed (CMD6): -110, retrying...

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000

mmc0: req done (CMD6): -110: 00000000 00000000 00000000 00000000

imx6 usb charger online:0

android_work: sent uevent USB_STATE=DISCONNECTED

fsl_gadget_disconnect_event: udc enter low power mode

ehci_fsl_bus_resume begins, Host 1

ehci_fsl_bus_resume ends, Host 1

usb usb2: usb_resume_device: status 0

ラベル(2)
0 件の賞賛
返信
1 解決策
9,700件の閲覧回数
ningli
Contributor III

Hi,

everybody,i fixed this bug,

static const struct esdhc_platform_data mx6_evk_sd1_data __initconst = {

        .always_present = 1,

        .cd_gpio                = -1,//MX6_BRD_SD1_CD,

        .wp_gpio                = -1,

        .support_8bit                = 1,

        .keep_power_at_suspend        = 1,

        .delay_line                = 0,

        .support_18v                = 1,

        .platform_pad_change = plt_sd_pad_change,

        .cd_type = ESDHC_CD_PERMANENT,

};

modify .support_18v                = 1, to   .support_18v                = 0,

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
9,701件の閲覧回数
ningli
Contributor III

Hi,

everybody,i fixed this bug,

static const struct esdhc_platform_data mx6_evk_sd1_data __initconst = {

        .always_present = 1,

        .cd_gpio                = -1,//MX6_BRD_SD1_CD,

        .wp_gpio                = -1,

        .support_8bit                = 1,

        .keep_power_at_suspend        = 1,

        .delay_line                = 0,

        .support_18v                = 1,

        .platform_pad_change = plt_sd_pad_change,

        .cd_type = ESDHC_CD_PERMANENT,

};

modify .support_18v                = 1, to   .support_18v                = 0,

0 件の賞賛
返信
9,700件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

one can try to erase eMMC then program with mfg tools

sudo dd if=/dev/zero of =/dev/sdx

what is about linux, is it able to boot ?

0 件の賞賛
返信
9,700件の閲覧回数
ningli
Contributor III

Hi ,

i  find one bbs https://community.nxp.com/message/473435#comment-477781​ descripted same problem with my. Can you give me oen copy of the kernel v 3.10.17 code. thanks !!

my email is [email protected]

0 件の賞賛
返信
9,700件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信
9,700件の閲覧回数
ningli
Contributor III

i think maybe i should use this  script  <CMD state="Updater" type="push" body="$ dd if=/dev/zero of=/dev/mmcblk0 ">

but this can't execute sucessful

0 件の賞賛
返信
9,700件の閲覧回数
ningli
Contributor III

i didn’t try on linux。 but another anroid img can boot up normally,i don‘t have this img’s code。 so i think mmc driver code‘s problem is most probably。

0 件の賞賛
返信
9,697件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ning

please use mfg tool for eMMC programming, as it automatically do all partition

formatting, refer to attached Android Guide sect.4.1.2 Downloading images with MFGTool

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
9,697件の閲覧回数
ningli
Contributor III

Hi igorpadykov,

i use mfg tool all the time! But, the problem still there! Is there any other method?

0 件の賞賛
返信
9,697件の閲覧回数
ningli
Contributor III

Hi igorpadykov,

i don't understand your meaning . Did  you mean i download images using wrong way?

0 件の賞賛
返信