can share the same external flash memory for 2 processors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

can share the same external flash memory for 2 processors

2,199 次查看
mohammed_saleh
Contributor I

In one of our RFQ, We are using MIMX8MN2DVTJZAA as the primary processor and MIMXRT1051DVJ6B  from NXP USA Inc as to the secondary processor.

Can anyone please help us to solve the below query?

 

Whether two processors can share the same external flash memory?

0 项奖励
回复
3 回复数

2,067 次查看
nxf54947
NXP Employee
NXP Employee

Hello [email protected]‌,

Could you please specify which external flash memory interface are you willing to use?

Regards,



0 项奖励
回复

2,067 次查看
mohammed_saleh
Contributor I

Hi,

Please find the flash part below

W25N01GVZEIG TR: IC FLASH 1G SPI 104MHZ 8WSON

Regards,

Mohammed Saleh

0 项奖励
回复

2,066 次查看
nxf54947
NXP Employee
NXP Employee

Hello [email protected]‌,

I've found that your query was already answered in the post below. Feel free to reopen any of two threads if needed.


Processor can share the same external flash memory?


Kind regards,

Ruben

0 项奖励
回复