can share the same external flash memory for 2 processors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

can share the same external flash memory for 2 processors

2,204件の閲覧回数
mohammed_saleh
Contributor I

In one of our RFQ, We are using MIMX8MN2DVTJZAA as the primary processor and MIMXRT1051DVJ6B  from NXP USA Inc as to the secondary processor.

Can anyone please help us to solve the below query?

 

Whether two processors can share the same external flash memory?

0 件の賞賛
返信
3 返答(返信)

2,072件の閲覧回数
nxf54947
NXP Employee
NXP Employee

Hello [email protected]‌,

Could you please specify which external flash memory interface are you willing to use?

Regards,



0 件の賞賛
返信

2,072件の閲覧回数
mohammed_saleh
Contributor I

Hi,

Please find the flash part below

W25N01GVZEIG TR: IC FLASH 1G SPI 104MHZ 8WSON

Regards,

Mohammed Saleh

0 件の賞賛
返信

2,071件の閲覧回数
nxf54947
NXP Employee
NXP Employee

Hello [email protected]‌,

I've found that your query was already answered in the post below. Feel free to reopen any of two threads if needed.


Processor can share the same external flash memory?


Kind regards,

Ruben

0 件の賞賛
返信