I tested and got good working result from follow link:
And then, I would like to test with local mp4 files
So, I ran below cmd:
gst-launch-1.0 clockselect. \( clock-id=realtime \
filesrc location=sintel_trailer-480p.mp4 ! qtdemux ! h264parse config-interval=-1 ! \
avtpcvfpay processing-deadline=20000000 mtu=1400 mtt=2000000 tu=125000 streamid=0xAABBCCDDEEFF000A ! \
avtpsink ifname=eth1.5 priority=3 processing-deadline=20000000 \)
But, i got error:
0:00:00.087338126 1992 0xaaaaf02a5c40 WARN basesrc gstbasesrc.c:3688:gst_base_src_start_complete:<filesrc0> pad not activated yet
Pipeline is PREROLLING ... Pipeline is PREROLLED ... Setting pipeline to PLAYING ... New clock: DebugGstSystemClock Got EOS from element "clockselect0". Execution ended after 0:00:00.544463000 Setting pipeline to NULL ... Freeing pipeline ...
Could you give any advise to fix this issue?
Thanks.
I am trying to run a c++ application on a i.mx8mp with Kirkstone Linux that has configured a Gstreamer pipeline with a avtpsrc -> avtpcvfdepay -> h26parse -> avdec_h264 -> videoconvert -> vvideorate -> vpuenc_hevc -> appsink
The pipline starts running with no problems, but when it starts to receive the AVTP packets over the Base-T1 ethernet port, it begins to complain as follows:
GStreamer-App-CRITICAL **: 16:58:57.771: gst_app_src_end_of_stream: assertion 'GST_IS_APP_SRC (appsrc)' failed
Is there some setting in the avtpsrc plugin that I am missing or is there something wrong with my AVTP stream?
Any suggestions are greatly appreciated.
Anyone can guide me related to TSN QDISC setup.
Like if we are not doing this setup what will happen, we will able to run talker/listner application or not.
I am aksing this because i don't have I210 NIC card i have marvel card installed in my intel acrn tiger lake board by which i am able to do timesyncronization. I don't know about the number of queues available in this NIC card and how to configure this.
Thanks.
HI @OliverSJ
I am also getting same error while tying to stream video from talker to listner by using .mp4 file.
My setup:Intel tiger lake board (With Marvel NIC)
Do you find any solution for this issue or not? Please guide me if you got any solution.
Thanks.
Hi @OliverSJ,
Thank you for contacting NXP Support.
Are you working on our EVK or custom board?
What is you BSP version?
It seems that there is a problem related to the clock and it could be an erroneous clock setting.
Please send me the information to check in detail.
Have a great day!
Hi brian!
Thank you for your support.
I used i.MX 8M PLUS EVK.
and I flashing below image (downloaded from imx website):
L5.4.24-2.1.0_images_MX8MMEVK.zip
And I've changed some of libraries and kernel&dtb images by referring to below link for AVB/TSN:
If you want to more detail, please reply here
Hi @OliverSJ,
Based on my tests and research, it seems that this format is unsupported. That community article is valid for the formats that have been described in the document.
I hope this information will be helpful.
Have a great day!