can not boot from emmc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can not boot from emmc

1,532 Views
jiejia
Contributor III

I download image to my custom board similar to the I.MX6Q Sabresd using mfgtool. One board can boot successfully. Another board failed to execute the uboot, but I sure all the image had be downloaded by mfgtool. However, it always detect the HID-compliant device in mfgtool after reset my board.   I download my uboot.bin to ddr, and enter the uboot command line. I change the uboot command line parameters to make it boot from emmc, and it can enter rootfs successfully.  By the way, Boot Select Table is the same as another board. I can detect the pulse of SD4_CMD from the oscilloscope.


Have I missed anything?

0 Kudos
Reply
1 Reply

1,280 Views
igorpadykov
NXP Employee
NXP Employee

Hi jie

one can try to change eMMC pad settings, such as drive strength

or BOOT_CFG2[2]=1 Apply value per fuse field MMC_DLL_DLY[6:0]

find best value experimentally. Please check Table 8-15 IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply