camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

camera

2,827 Views
1990rahulreddy
Contributor IV

I am working on Freescale i.MX6Q SABRE SDB Board. Can anyone suggest mi camera which has driver available, so that I can plug it & use. or which is best camera for Machine Vision application

Labels (3)
Tags (1)
0 Kudos
Reply
3 Replies

2,525 Views
1990rahulreddy
Contributor IV

Which one is BEsT. OV5640 or OV5642.

Please, help mi to inspect more & choose the BEST

0 Kudos
Reply

2,525 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rahul

OV5640,42 are supported in FSL BSPs for SABRE SD boards, modules

OV05640-MRFL-A00A/ OV5462-MRSL-A01A

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,526 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

You can buy one of them in the links of this page:

http://www.findchips.com/search/ov05640

Luis

0 Kudos
Reply