camera preview on screen without Linux or any other OS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

camera preview on screen without Linux or any other OS

1,321件の閲覧回数
balakrishnanven
Contributor I

Hi Yuri,

We are using Analog camera with TVP5150 decoder connected to csi0 . We would like to show camera preview on screen without Linux or any other OS, with just bare metal code.

Can you please provide the camera preview bare metal code and help us?

I have created a support request: 00120422.

Thank you very much.

0 件の賞賛
返信
1 返信

1,219件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  As I see the request 00120422 has been answered by Jimmy.
You may also use the following link :

swp-report/iMX6_Platform_SDK at master · backenklee/swp-report · GitHub 

Please refer to Chapter 21 (Configuring the Camera Preview Driver) and
Chapter 18 (Configuring the IPU Driver) of "iMX6_Firmware_Guide.pdf".

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信