camera preview on screen without Linux or any other OS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

camera preview on screen without Linux or any other OS

1,318 次查看
balakrishnanven
Contributor I

Hi Yuri,

We are using Analog camera with TVP5150 decoder connected to csi0 . We would like to show camera preview on screen without Linux or any other OS, with just bare metal code.

Can you please provide the camera preview bare metal code and help us?

I have created a support request: 00120422.

Thank you very much.

0 项奖励
回复
1 回复

1,216 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  As I see the request 00120422 has been answered by Jimmy.
You may also use the following link :

swp-report/iMX6_Platform_SDK at master · backenklee/swp-report · GitHub 

Please refer to Chapter 21 (Configuring the Camera Preview Driver) and
Chapter 18 (Configuring the IPU Driver) of "iMX6_Firmware_Guide.pdf".

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复